Suggested Categories

Showing 3550 products in 407 families
Products Here
Technical Notes

Nominal PID Constants for the Newport 350B Temperature Controller

When setting PID constants for a temperature controller, various combinations of values can be used to optimize performance for a given application.

Manual

764H Series LD Mount User Manual

The Model 764H series High Power Laser Diode Mounts are industrial grade Cold Plates adapted for research applications. These mounts are optimized with Newport’s temperature controllers, …

Manual

3700 Temperature Controller User Manual

Model 3700 Temperature Controller is a result of Newport’s continuing commitment to deliver innovative solutions that enable its customers’ success.

Videos

6100 LIV Characterization Demonstration

An overview of performing a LIV characterization using a model 6100 Laser Diode and Temperature Controller and other equipment from Newport Corporation.

Application Notes

Temperature Monitoring Using a Simple GUI

This application note describes a simple Graphical User Interface (GUI) developed to allow the users to monitor thermoelectric current ITE and thermoelectric cooler temperature T over …

Technical Notes

Temperature Controllers: Setting PID Gains for the 6100 and 3700

One of the most difficult to understand and confusing processes when working with temperature control of laser diode systems is the choice of the PID gains to be used. The goal of this …

Videos

Quantum Efficiency Measurements: Fundamentals for Solar Cell Research (Part Two)

In part two of this series, representatives from MKS Newport present an in-depth discussion on equipment and test configurations used for cutting-edge cell development such as perovskites …

Technical Notes

Newport ESP Technology

Newport controllers automatically configure ESP-compatible stages delivering true Plug-and-Play for a quick and safe start to positioning applications. Newport's ESP (Enhanced System …

Technical Notes

Newport Meter User Commands

List of manual user commands available for Newport power meters to enable remote control.

Videos

Newport Air Bearing Stage Solutions

High performance air bearing stage solutions for precision, repeatability and throughput offered in DynamYX®, HybrYX® and SinguLYS™ family.

Technical Notes

Newport Motion Control and EPICS

The staff at Argonne National Laboratory has developed software drivers to interface EPICS with Newport Motion Controllers. Controllers such as the XPS Series are playing vital roles …

Videos

Partner With Newport - Extended Version

From prototype through to production, see the benefits of partnering with Newport Corporation for custom optical mounts and translation stages.

Videos

Newport Motion 50 Year Anniversary

Looking back at 50 Years of precision motion control from Newport Corporation.

Technical Notes

Newport User Commands Revision 07

This document contains a description of the various commands that are used for remote control of the new line of Newport meters (843-R-USB, 1919-R, 841-PE-USB, 844-PE-USB, 845-PE-RS, …

Videos

Newport Integrity VCS Vibration Control System

Integrity VCS Vibration Control System, the new standard for basic optical applications.

Videos

Newport Hardware for Fiber Alignment Applications

This video demonstrates a number of examples of Newport Motion and Photonics products used in Fiber Alignment. Newport can supply many options from its standard product line for Fiber …

Literature

Newport Custom Optics Fabrication Capabilities Matrix

Newport offers advanced optics component technologies to OEM customers in markets ranging from semiconductor equipment and biomedical instruments to industrial, aerospace and defense …

Videos

Newport Cornerstone 130B 1/8m Monochromator

Newport’s Cornerstone 130B 1/8m monochromator is ideal for research and OEM applications where speed and reliability are essential. Based on the same optical design as its predecessor, …

Videos

Introducing Newport Solutions for Photovoltaic Manufacturing

Overview of Newport's solution portfolio for photovoltaic manufacturing from lasers, to motion control, to optical components, to the SolaryX™ family of PV scribe tools.

Videos

University of Arizona Chooses Newport Optical Tables

The University of Arizona chooses Newport Optical Tables as the Foundation for their New Grand Challenges Research Building.