Showing 398 products in 65 families
In Stock
$146

Products Here
Manual

Broadband Faraday Isolator User Manual

Newport’s ISO-05-800-BB and ISO-08-800-BB Faraday Isolators are essentially uni-directional light valves or spectrally selective one-way mirrors. They are used to protect a laser source …

Application Notes

System-in-Package (SiP) Manufacturing

As traditional chip-level scaling is reaching its limits, an alternative is system-level scaling through system-in-package (SiP). Also known as 2.5D/3D packaging, SiP enables heterogenous …

Manual

Advanced Fiber Optic Kit Instruction Book TOC

The Project Workbook (FK-ADV-TEXT), when compared to its introductory predecessor Projects in Fiber Optics, is written as a technically more advanced manual, geared towards students …

Technical Notes

Beam Expanders

Simple beam expanders are essentially telescopes which, in their most basic forms, consist of two lenses. The input beam is assumed to be collimated. The first lens must have a diameter …

Technical Notes

Laser Beam Spatial Profiles

The irradiance distribution of a laser beam is determined by the transverse modes that exit the laser cavity. Typically, the lowest-order transverse mode (TEM00) is selected for emission …

Technical Notes

Laser Beam Profile Measurement

Given the different types of laser beam spatial distributions and their evolution as they propagate in free space and through optical elements, measurement of the beam profile is critical …

Application Notes

Non-Contact Laser Beam Measurement

A non-contact method developed by MKS Ophir is based on Rayleigh scattering. Rayleigh scattering is the scattering of light by particles that are smaller than the radiation's wavelength, …

Tutorials

Introduction to Polarizers

The interaction of light with the atoms or molecules of a material is wavelength dependent. A consequence of this dependence is the resonant interactions related to material dispersion. …

Technical Notes

Fundamentals of Spatial Filtering

Spatial filters provide a convenient way to remove random fluctuations from the intensity profile of a laser beam. This greatly improves resolution — which is especially critical for …

Technical Notes

Polarization Control with Optics

Precise control of polarization behavior is necessary to obtain optimal performance from optical components and systems. Characteristics such as reflectivity, insertion loss, and beamsplitter …

Application Notes

Super-Resolution Microscopy (STED and PALM)

One super-resolution approach is called stimulated emission depletion (STED) microscopy. This technique uses a confocal microscope and a diffraction limited excitation beam that is …

Technical Notes

Light-Matter Interactions in Lasers

Light is generated from a laser as a result of the following process: electrons in a material move from an excited energy level to a lower-lying energy level and produce photons that …

Application Notes

Real-Time Laser Power Measurement

Only when performing optimally can laser systems guarantee the most cost-effective production of high-quality components. Even the smallest deviations in beam adjustment or focal position …

Application Notes

Raman Spectroscopy (CARS and SRS)

In CARS microscopy, the pump and Stokes beams are tightly focused into the sample and a CARS image is generated by scanning either the sample or the laser beams.

Application Notes

Flow Cytometry Overview

Flow cytometry is an analytical technique that can rapidly measure the properties of individual cells or particles as they pass through a beam of light, typically a laser.

Selection Guides

Ophir Laser Beam Profilers

As the trusted leader in laser beam profiling, Ophir provides a complete range of solutions for beam characterization for any wavelength, at any power and for any beam diameter. The …

Technical Notes

Gaussian Beam Optics

The Gaussian has no obvious boundaries to give it a characteristic dimension like the diameter of the circular aperture, so the definition of the size of a Gaussian is somewhat arbitrary. …

Selection Guides

Optical Beamsplitter Guide

An Optical Beamsplitter is an optic or optical device that is used to split a beam of light in two. Newport offers a wide variety of Beamsplitters in various shapes. Circular beamsplitters, …

Technical Notes

Beam Shaping with Cylindrical Lenses

Cylindrical Lenses focus or expand light in one axis only. They can be used to focus light into a thin line in optical metrology, laser scanning, spectroscopic, laser diode, acousto-optic, …

Selection Guides

Beamsplitting Mounts Guide

Plate beamsplitter mounts are designed to effectively manage beam transmission, beamsplitting angle and paths of both the reflected and transmitted beams.