Showing 515 products in 23 families
Products Here
Application Notes

The Michelson Interferometer Experimental Setup

Albert A. Michelson won the 1907 Nobel Prize in Physics “for his optical precision instruments and the spectroscopic and metrological investigations carried out with their aid.” One …

Application Notes

Phase-Shifting Interferometry for Determining Optical Surface Quality

Determining the surface quality of a critical component—the deviation from the intended shape whether flat, spherical, etc.—is crucial to high-precision manufacturing. Traditional methods …

Videos

Picomotor demo using interferometer

A demonstration of the New Focus Picomotor using an interferometer. The Picomotor allows for accurate, minute adjustments that cannot be achieved using a manual micrometer.

Application Notes

Testing MEMS-based Accelerometers in GPS Navigation System with a Custom 2-Axis Gimbal

Built from two, high-precision RV series rotary stages, the inner stage providing roll motion and the outer stage assembly providing elevation, the gimbal is an ideal platform to test …

Application Notes

Theory of Lloyd’s Mirror Interferometer

There are two principal methods for producing coherent sources for interferometry. One uses the division of wavefront, as in the Young’s double slit experiment. The second divides the …

Technical Notes

Interfacing an Interferometer Encoder to an XPS Controller

This tech note describes how to configure and setup a Renishaw Interferometer Encoder with an XPS controller. This can help with both diagnostics and measurement for an enhanced level …

Videos

Interferometric Testing Wavefront Distortion

Actual (not simulated) interferometric testing of our LWD Mirror Mounts demonstrate that the low-stress mirror mounting clamp significantly reduces wave front distortion. In this video, …

Technical Notes

Optics Based Research - The Need for Vibration Isolated Rigid Support Structures

Advanced equipment and processes have made it possible to investigate phenomena with dimensions measured in nanometers. For example, phase-shifting optical interferometers can now measure …

Application Notes

Tunable Lasers Applications to Spark Your Imagination

Interferometry is widely used to make precision length and displacement measurements ranging from less than a nanometer to tens of meters. Researchers used our 630-nm TLB-6304 laser …

Manual

Vision IsoStation User's Manual

The Vision IsoStation vibration isolated workstation provides an ideal working platform for vibration influenced devices such as interferometers, microscopes, and balances.

Manual

SmartTable OTS User's Manual

The Newport SmartTable® OTS™ Vibration Isolation Workstation provides an ideal working platform for vibration influenced devices such as interferometers, microscopes, and balances.

Application Notes

Polarite Polarization Controllers

In fiber optic communication and sensing systems, many devices, such as interferometers and electro-optic modulators, are polarization sensitive. In order for these polarization sensitive …

Technical Notes

Laser Wavelength Measuring Using a Colored Glass Filter

ILX Lightwave has developed a wavelength measurement technology based on the transmission verses wavelength characteristics of colored filter glass. (See Graph 1). While some wavelength …

Application Notes

Long Scan Autocorrelator

When phase information of the pulse is not required, autocorrelation is the simplest and most affordable method for determining pulse width. The principle of operation is based on recording …

Manual

Integrity VCS Optical Tables User's Manual

The Newport Integrity VCS™ Vibration Control System provides an ideal working platform for vibration influenced devices such as interferometers, microscopes, and balances.

Manual

LQx Series Laser Diode Modules User's Manual

Newport’s LQx Series Laser Diode Light Source Modules can be used in analytical, industrial and biomedical applications, such as spectroscopy, interferometry, machine vision, marking, …

Application Notes

Collimation Tester

The Newport Collimation Tester 20QS20 makes use of a technique called “Shearing Interferometry.” This is a null method used to test the collimation of laser light whose coherence length …