Showing 169 products in 17 families
Products Here
Manual

Broadband Faraday Isolator User Manual

Newport’s ISO-05-800-BB and ISO-08-800-BB Faraday Isolators are essentially uni-directional light valves or spectrally selective one-way mirrors. They are used to protect a laser source …

Manual

Mid-IR Faraday Isolators User's Manual

Our Mid-IR Faraday optical isolators act essentially as uni-directional light valves. They are used to protect a laser source near 2050 nm or 4550 nm from destabilizing feedback or …

Manual

MP ISO Faraday Isolators User's Manual

Newport Faraday Isolators are essentially uni-directional light valves, used to protect a laser source from destabilizing feedback or actual damage from back-reflected light.

Manual

LP ISO Faraday Isolator User's Manual

Newport's Faraday Isolators are uni-directional light valves used to protect a laser source from destabilizing feedback or actual damage from back-reflected light.

Manual

High Power Faraday Isolator User Manual (8 mm aperture)

Newport's Faraday Isolators are essentially uni-directional light valves. They are used to protect a laser source from destabilizing feedback or actual damage from back-reflected l …

Application Notes

Feedback Prevention with Optical Isolators

Because fiber is a high gain medium, any light that is inadvertently injected into the ultrafast oscillator, as well as into amplifiers, can degrade and potentially irreversibly affect …

Application Notes

Supercontinuum Generation in SCG-800

As a PCF based supercontinuum source, Newport offers the SCG-800. It is a pre-assembled device consisting of a polarization maintaining PCF designed for zero dispersion at 750 nm in …

Application Notes

Coherent Anti-Stokes Raman Scattering

Coherent Anti-Stokes Raman Scattering (CARS) was first reported in 1965 by Maker and Terhune as a method of spectroscopy for chemical analysis. CARS involve the interaction of four …

Tutorials

Photonic Crystal Fiber Basics

Photonic crystal fibers are generally divided into two main categories: Index Guiding Fibers that have a solid core, and Photonic Bandgap Fibers that have periodic microstructured elements …

Technical Notes

Fiber Optics: Photonic Crystal Fibers (PCFs) - Technical Note

PCFs are generally divided into two main categories: Index Guiding Fibers that have a solid core, and Photonic Bandgap Fibers that have periodic microstructured elements and a core …

Application Notes

Variable Attenuator for Lasers

This application note details a simple and cost effective solution for the continuous attenuation of laser output power. The attenuator kit described is based on a half waveplate and …

Application Notes

Mode Hopping in Semiconductor Laser Diodes

In this Application Note, we show that mode hopping is directly correlated to noise in the total intensity, and that this noise is easily detected by a photodiode. We also show that …

Literature

Vision IsoStation Brochure

The Vision IsoStation provides industry leading performance and more user friendly features and accessories than any other vibration isolation workstation. All of the features and accessories …

Manual

Vision IsoStation User's Manual

The Vision IsoStation vibration isolated workstation provides an ideal working platform for vibration influenced devices such as interferometers, microscopes, and balances.

Tutorials

Introduction to Polarizers

The interaction of light with the atoms or molecules of a material is wavelength dependent. A consequence of this dependence is the resonant interactions related to material dispersion. …

Selection Guides

Optical Workstation Guide

Applications of Newport vibration control workstations include microscopy, spectroscopy, inspection, photovoltaic measurement, etc. Vision IsoStation™ Optical Workstations are the ideal …

Application Notes

Measuring and Reducing Noise Using an LDX-3620B Ultra Low Noise Laser Diode Current Source

ILX Lightwave specifies the noise and ripple of every instrument with an rms current noise measurement. The purpose of this application note is to describe the procedure that is used …

Application Notes

Protecting Your Laser Diode

It’s been said that there are two types of researchers - those who have blown a laser diode and those who will. While that may be an exaggeration, it’s certainly true that today’s lab …

Technical Notes

Protecting Your Laser Diode

It’s been said that there are two types of researchers - those who have blown a laser diode and those who will. While that may be an exaggeration, it’s certainly true that today’s lab …