Technical Notes

Technical Notes

Motion Control Systems

In this technical note, motion devices are discussed first in the context of manual positioning. This discussion is equally applicable to automated positioning and motorized drivers …

Technical Notes

Fundamentals of Motion Control

Details regarding the various factors that impact the motion of these devices and how to characterize their positioning precision and accuracy are the subjects of this technical no …

Technical Notes

Optical Fiber Alignment

Good fiber alignment produces the highest coupling efficiency and therefore the least signal loss before assembly or packaging of an optical system.

Technical Notes

Linear Translation Stage Terminology

This glossary covers important terms related to linear translation stages.

Technical Notes

Motion Basics Terminology & Standards

The function of a stage is to constrain motion to a desired direction. For a linear stage, the desired motion is along an ideal straight line. Any motion in a constrained direction …

Technical Notes

Stage Components Considerations

Choosing the right positioning technology for an application is a complex task. There are numerous choices of linear stages, rotation stages and actuators and each product has its own …

Technical Notes

Linear Translation Stage Technology Guide

Each material used in the design of a linear translation stage has its own unique set of advantages and disadvantages. The following is a summary of the properties for the most common …

Technical Notes

Control Theory Terminology

Common motion systems use three types of control methods. They are position control, velocity control and torque control. The majority of Newport’s motion systems use position control. …

Technical Notes

TRA and TRB Series Compatibility with Manual Positioners and Mounts

Newport's TRA & TRB series miniature motorized linear actuator are offered in 6 mm, 12 mm and 25 mm travel versions with 60 N or 90 N load capacity.

Technical Notes

PZA12 Compatibility with Manual Positioners

Newport's PZA Ultra-High Resolution Actuator provides 12.5 mm travel with 50 N load capacity.

Technical Notes

LTA Series Compatibility with Manual Positioners and Mounts

Newport's LTA series actuators are offered in HS or HL version for 50/25 mm travel range with 50/120 N load capacity respectively.

Technical Notes

Motorized Actuator Compatibility with Manual Mirror Mounts

This note details the compatibility of Newport motorized actuators with our manually adjusted mirror mounts.

Technical Notes

Motorized Linear Actuator Compatibility Guide

Many Newport manual positioning products can be motorized by using Newport motorized precision actuators. Once the manual positioner is chosen for an application, use the tables below …

Technical Notes

Picomotor™ Compatibility with Manual Positioners

Many Newport manual positioning products can be motorized by using Newport motorized precision actuators. When very high precision, nano-scale linear positioning is required, a Piezo …

Technical Notes

Motion Electronics Design

Motion control systems consist of three main components: motion controller, motor driver or amplifier, and a motion device. The primary purpose of a motion controller is to control …

Technical Notes

Motion Controller GUIs

Newport has recently introduced new Graphical User Interfaces (GUIs) for the popular motion controllers. The new GUI simplifies the user experience and enables communication, stage …

Technical Notes

Motion Control Metrology Primer

In our continuing effort to provide the most accurate information to the research, defense and industrial communities, we have expanded many of our product specifications to reflect …

Technical Notes

Stage Motor Technical Information

All motorized Newport stages are optimized for use with Newport’s motion controllers and motor drivers to ensure plug-and-play compatibility, reliability and the ability to meet stated …

Technical Notes

Metrology and Acceptance Test Procedure

In today's world of shrinking feature sizes, nanometer-scale devices as well as higher accuracy and resolution requirements, it is critical to use the highest quality components available. …

Technical Notes

Open vs. Closed Loop Picomotor Control

Designed specifically for single-mode fiber positioning, the 561/562 Series meets the most difficult challenges in component engineering. The core of a single-mode fiber can be as small …

Page 1 of 3