The 68950 is a digital exposure system for research lamp sources. The system is a light intensity controller and digital timer in one. The light intensity controller maintains a constant light output from your arc, deuterium, or quartz tungsten halogen lamps, whereas the digital timer allows timed exposures and dose control. RS-232 communications allow computer controlled operation.
- Light intensity controller and digital timer in one
- Ensures stable long term output from arc, deuterium and QTH lamps
- Dose control
- RS-232 communications See All Features
| Compare | Description | Drawings, CAD & Specs | Avail. | Price | ||
|---|---|---|---|---|---|---|
![]() | 68950Digital Exposure System, Research Lamp Sources | In Stock |
Features
Correct for Lamp Output Variations with Age
Our lamp power supplies are highly regulated and operate lamps at constant current or power, even if the line voltage changes over a wide range. Even with lamp current constant, the light output of many lamps varies with age, filament or electrode erosion, gas adsorption or desorption, and, particularly for mercury lamps, ambient temperature. Both the total output and the distribution of power between the spectral lines from a mercury lamp change with temperature. These effects cause output variations with time, with different and sometimes pronounced frequency dependence. Even the relatively simple quartz tungsten halogen lamps exhibit output variations: evaporation and halogen cycle redeposition of tungsten constantly change the microstructure of the filament. The 68950 corrects for these lamp output changes, maintaining a constant, long term output, from the lamp.
Ideal Optical Set-up
We recommend that you rod mount the light sensor as shown in Fig. 3, using a 5° Wedge to split off part of the beam. The normal surface reflection off the substrate is enough to "pick-off" a portion of the beam for monitoring by the 68950 sensor. You can also use a beamsplitter at 45°, but you may need to attenuate the light hitting the sensor with an aperture, diffuser or filter, depending upon the reflectance of the beamsplitter. The 7123 Mount holds a 1 inch (25.4 mm) diameter optic at the input of the light sensor. Another method of monitoring the light output, if you have plenty of light to spare, is to use an integrating sphere at the output of the source, and mount the light sensor on one of the sphere’s ports.
Monitors and Adjust Light Output
The 68950 is made up of a light sensing head and a controller. The silicon based light sensor is temperature stabilized to maintain complete independence from temperature variations and monitors part of the light source's output. The controller constantly compares the recorded signal to the set level and changes the power supply output as the lamp ages or as other conditions cause a change.
Built-in Digital Timer
The built-in digital timer controls any of our electronic shutters for timed exposure applications. Accurate, repeatable timed exposures down to 2 ms are possible. The Digital Exposure System for Research Sources, model 68950, doesn't directly drive the shutter, but rather provides a TTL output signal for the shutter controller, which is a part of the shutter system. We also offer Electronic Safety Shutters.
Adapter Kits for Oriel® Lamp Housings
For convenience, you can mount the sensor directly to the lamp housing. The
Accessories
Compatible Lamp Housings
| Compare | Description | Drawings, CAD & Specs | Avail. | Price | ||
|---|---|---|---|---|---|---|
![]() | 67011QTH Lamp Housing, Research, 10-250 W, F/1 FS Asphere, Collimated | 4 Weeks | ||||
![]() | 60000Lamp Housing, Q Series, Adjustable Reflectors & Up to 4 Condensers | 2 Weeks | ||||
![]() | 66881QTH Lamp Housing, Research, 10-250 W, F/0.85 Borofloat Glass, Collimated | In Stock | ||||
![]() | 67009QTH Lamp Housing, Research, 10-250 W, F/2.2 FS Asphere, Collimated | 2 Weeks | ||||
![]() | 66885QTH Lamp Housing, Research, 600-1000 W, F/1, 2 Element FS, Collimated | 6 Weeks | ||||
![]() | 67001Arc Lamp Housing, Research, 50-500 W, F/2.2 Asphere, 1.5 Inch Flange | 6 Weeks | ||||
![]() | 66902Arc Lamp Housing, Research, 50-500 W, F/1 2 Element Plano-Convex, 1.5 Inch Flange | |||||
![]() | 66921Arc Lamp Housing, Research, 450-1000 W, F/1 2 Element Plano-Convex, 2 Inch Flange | 4 Weeks | ||||
![]() | 66901Arc Lamp Housing, Research, 50-500 W, F/1.5 Plano-Convex, 1.5 Inch Flange | |||||
![]() | 66923Arc Lamp Housing, Research, 450-1000 W, F/0.7, 4 Element Aspherab, 3 Inch Flange | |||||
![]() | 67005Arc Lamp Housing, Research, 50-500 W, F/1 Asphere, 1.5 Inch Flange | 4 Weeks |
Resources
Manuals
Oriel 6895X Digital Exposure Systems User Manual(657.2 kB, PDF)