Page view updated with the selected options.
Showing 1 - 20 of 28 Technical Notes
undefined

Technical Notes

Reliable Spectroradiometry

Reliable spectroradiometry takes a lifetime of work and attention to master. Unreliable spectroradiometry is much easier to accomplish1 all it takes is missing a single critical point, ...
undefined

Technical Notes

Introduction to FTIR Spectroscopy

An FT-IR Spectrometer is an instrument which acquires broadband NIR to FIR spectra. Unlike a dispersive instrument, i.e. grating monochromator or spectrograph, FT-IR Spectrometers collect ...
undefined

Technical Notes

Simulation of Solar Irradiation

Oriel® Solar Simulators provide the closest spectral match to solar spectra available from any artificial source. The match is not exact, but better than needed for many applications. ...
undefined

Technical Notes

Solar Simulator Standards

A solar simulator is a light source that approximates the illumination of natural sunlight. The ability of a solar simulator to approximate natural sunlight is based on three criteria: ...
undefined

Technical Notes

Information on Spectral Irradiance Data

The radiometric data shown at the end of this section was measured in our Standards Laboratory. The wavelength calibrations are based on our spectral calibration lamps. Irradiance data ...
undefined

Technical Notes

Optical Radiation Terminology and Units

There are many systems of units for optical radiation. In this tutorial, we try to adhere to the internationally agreed CIE system. The CIE system fits well with the SI system of units. ...
undefined

Technical Notes

Arc Lamp Spectral Irradiance Data

Spectral irradiance data is shown below for our Arc Lamps. You can click on the curve for a larger image, or on a model number for complete information on a specific arc lamp. Spectral ...
undefined

Technical Notes

Optical Detection Systems

In a typical photo-research system, a detector measures the radiant intensity used to evoke photo-response in a sample or the radiant intensity produced by the sample in response to ...
undefined

Technical Notes

Oriel® Calibration Light Sources

The most accurate and economical method of wavelength calibration is the spectral calibration lamp. We offer lamps to cover wavelengths from below 185 nm to over 2.5 µm. Be sure to ...
undefined

Technical Notes

Solar Simulator Definitions of Characteristics

This glossary briefly defines the terms and units most frequently used in technical discussions around solar simulation.
undefined

Technical Notes

Solar Simulator Sample Calculations

The spectral irradiance at any wavelength, Eλ, is in units of watts per square meter per nm (W m-2 nm-1). The value is a measure of the flux per nm at the specified wavelength incident ...
undefined

Technical Notes

LEDs Drive the Latest Innovation in Solar Simulator Technology

Newport's PZA Ultra-High Resolution Actuator provides 12.5 mm travel with 50 N load capacity.
undefined

Technical Notes

Using Spectral Irradiance Curves

Here we describe our spectral irradiance curves. Again, we caution you on the need for testing of the final configuration particularly when the “total radiation budget” for the system, ...
undefined

Technical Notes

Oriel Discontinued & Obsolete Products

These discontinued products are no longer sold by Oriel, but are typically supported for three years from the date on which they were discontinued. Repairs and calibrations are available ...
undefined

Technical Notes

Coupling a Fiber to the MS257

Below is a list of Oriel's standard families of fiber optic cables and liquid light guides, and the appropriate adapters to couple them to Oriel® Instruments MS257™ 1/4 m Monochromator ...
undefined

Technical Notes

Solar Simulator Spectral Irradiance Data

Spectral irradiance data is shown below for our Solar Simulators. You can click on the curve for a larger image, or on a model number for complete information on a specific solar s ...
undefined

Technical Notes

Solar Simulator Curve Normalization

To simplify visual comparison of our simulators' curve shapes with the shapes of the standard solar spectra curves, we scale the measured simulator output, without changing the sha ...
undefined

Technical Notes

Bandpass of a Spectrograph

With a spectrograph, the term bandpass refers to the entire wavelength range in the long strip output to the detector. Thus the bandpass in a spectrograph is very wide, limited only ...
undefined

Technical Notes

Improving Detector Performance

The constantly improving technology of detectors and wide selection of materials and detection methods allows most light detection needs to be satisfied by fairly simple systems. At ...
undefined

Technical Notes

QTH Lamp Spectral Irradiance Data

Spectral irradiance data is shown below for our QTH lamps. You can click on the curve for a larger image, or on a model number for complete information on a specific QTH lamp. Spectral ...
Page 1 of 2