Language Selector
Product Comparison

Choose products to compare anywhere you see 'Add to Compare' or 'Compare' options displayed.

Oriel® Calibration Light Sources

 

We offer various sources for use as calibration standards. We group them into two families:

Calibrated Irradiance Sources

  • Broadband, continuum sources
  • Carefully characterized spectral irradiance, traceable to NIST
  • Used as transfer standards to calibrate detection systems
  • Also used to cross-calibrate other lamps, or to irradiate a sample with a known power density.

Spectral Calibration Lamps

  • Produce narrow spectral lines
  • Used for wavelength calibration of spectral instruments (i.e. monochromators, spectrographs, spectral radiometers)

Choosing a Calibration Package

Although the two lamp families (Calibrated Irradiance Sources and Spectral Calibration Lamps) have decidedly separate purposes, they are often used together to completely calibrate a system. To achieve the highest accuracy, we suggest you use a spectral line lamp for wavelength calibration, then a calibrated irradiance lamp with a stabilized, radiometric power supply for power level calibration. If utmost accuracy is not crucial, our Hg(Ar) spectral calibration lamps may be used for spectral calibration and to determine relative power level calibration.

Uncertainties

The most important figure of merit for a calibration source is its accuracy. Accuracy is often stated using uncertainties that describe any possible variation from the true values. For some of our lamps you will find uncertainty values; use these values as a comparison to other products and as a guide for the error analysis of your own system.

Spectral Calibration Lamps

The most accurate and economical method of wavelength calibration is the spectral calibration lamp. We offer lamps to cover wavelengths from below 185 nm to over 2.5 µm.

Wavelength Uncertainty

These lamps emit line spectra when electrons residing in some excited energy level fall to a more stable energy level. The levels themselves are distinct states defined by the rest masses of atomic particles and the quantized charge of those particles. Therefore, a given chemical element may only emit radiation of specific wavelengths. Because this excitation and emission is a well-understood and documented process, the wavelengths are considered to be absolute and have been documented extensively. Environmental conditions such as dramatic temperature changes and the existence of strong electric or magnetic fields may cause a small shift in the location of some spectral lines. We have found that reasonable laboratory conditions produce emission spectra exactly as stated in the descriptions here.