Showing 19 products in 10 families
In Stock
$525

Products Here
Application Notes

Near Field Imaging of a Laser Diode

This note describes the result of an experiment performed on near field imaging of a laser diode emission pattern at the output facet. The purpose of the experiment was to provide a …

Application Notes

Thermal Imaging

Thermal imaging techniques involve discriminating between various objects in a scene based on their respective differences in temperature.

Technical Notes

Laser Beam Profile Measurement

Given the different types of laser beam spatial distributions and their evolution as they propagate in free space and through optical elements, measurement of the beam profile is critical …

Videos

LBP2 Laser Beam Profiler Datasheet

The Newport ACGP Silent Air Compressor is powerful, ultra-quiet and ideal for Newport’s vibration isolators.

Application Notes

Perovskite Processing

Perovskite solar cell manufacturing is a roll-to-roll process. Part of the process involves removing very narrow portions of thin-film layers of material in a multi-film stack without …

Application Notes

AWARE - Wide Field of View Camera

Recent advances in imaging technology coupled with an increasing demand in defense and security control have made it possible to deploy camera sensors in target tracking applications …

Solution

OLED Manufacturing Solutions

Energy efficient OLED panels are thin and flexible while offering superior image quality with faster response times than standard LED or LCD displays.

Application Notes

System-in-Package (SiP) Manufacturing

As traditional chip-level scaling is reaching its limits, an alternative is system-level scaling through system-in-package (SiP). Also known as 2.5D/3D packaging, SiP enables heterogenous …

Technical Articles

Two-Photon Polymerization-From the Inside Out

Additive manufacturing and 3D computer-aided design (CAD) have radically altered how prototype, developmental and customized mechanical components are created. Now the landscape is …

Application Notes

Workstation for Laser Direct-Write Processing

Lasers exhibit a number of features that makes them unique sources of energy for several material processing methods. For example, they are indispensable tools for drilling, welding, …

Application Notes

Light Sources in Mars Simulation Chamber

Scientists at the Kennedy Space Center, FL used Oriel® Light Sources in their Mars Simulation Chamber (MSC). The MSC was designed to accurately maintain the pressure (7 mb). temperature …

Manual

IRV2 Infrared Viewers Instruction Sheet

The IRV2 is a high performance infrared viewer designed to observe radiation emitted by infrared sources.

Technical Articles

CMOS Cameras Allow Robust Active Stabilization of Laser Beams - Laser Focus World

Accurate measurement of the position of a laser beam can be achieved in several ways, each with its strengths and weaknesses. A comparison of these has resulted in an active beam-stabilization …

Application Notes

Aspheric Laser Beam Reshaper Applications Guide

The Aspheric Laser Beam Reshaper, or reshaper for short, is a pair of plano-convex aspheric lenses which perform a deterministic geometrical transformation of the optical laser beam …

Tutorials

Light Collection and Systems Throughput

This discussion is restricted to the general use of Incoherent Light Sources, such as arc lamp or quartz tungsten halogen sources. Diffraction and coherent effects are excluded. The …

Technical Notes

Replication Justification

Flat mirrors made of Pyrex or metal from 1 to 1/10 wave accuracy is a good application for replication. Mirrors made from float glass to 2 waves/inch irregularity that can be made by …

Solution

Lithium-Ion Battery Manufacturing Solutions

The global demand for lithium-ion batteries has been growing for a number of years, and this growth isn’t going to stop. Laser manufacturing enables next-generation battery designs …

Application Notes

Three-Dimensional Microfabrication by Two-Photon Polymerization

Two-photon polymerization is a serial process for the fabrication of three-dimensional microstructures. Because of its ability to produce geometries with no topological constraints …

Technical Notes

Oriel Discontinued & Obsolete Products

These discontinued products are no longer sold by Oriel, but are typically supported for three years from the date on which they were discontinued. Repairs and calibrations are available …

Application Notes

Vat Polymerization

In vat polymerization systems—including stereolithography (SLA) and digital light processing (DLP)—a UV laser constructs an object in a vat of a liquid photopolymer resin by curing …