Page view updated with the selected options.
Tutorials
Fiber Optic Basics
Optical fibers are circular dielectric wave-guides that can transport optical energy and information. They have a central core surrounded by a concentric cladding with slightly lower ...
Tutorials
Light Collection and Systems Throughput
This discussion is restricted to the general use of Incoherent Light Sources, such as arc lamp or quartz tungsten halogen sources. Diffraction and coherent effects are excluded. The ...
Tutorials
Laser Diode Technology
Low-power laser diodes come in a variety of packages. Most have a monitor photodiode integrated with the laser diode. Generally, laser diodes emit light from both ends of their cavity. ...
Tutorials
Optical Power Measurement
When a photon hits the photodiode material, it may generate an electron-hole pair depending on the quantum efficiency of the device. Quantum efficiency is dependent on many factors, ...
Tutorials
PMManager™ Power Meter Application Software
PMManager is a powerful application software controlling and taking measurement data, compatible with models 1919-R, 843-R-USB, 844-PE-USB and 845-PE-RS.
Tutorials
Introduction to Polarizers
The interaction of light with the atoms or molecules of a material is wavelength dependent. A consequence of this dependence is the resonant interactions related to material dispersion. ...
Tutorials
Introduction to Waveplates
The interaction of light with the atoms or molecules of a material is wavelength dependent. A consequence of this dependence is the resonant interactions related to material dispersion. ...
Tutorials
Photonic Crystal Fiber Basics
Photonic crystal fibers are generally divided into two main categories: Index Guiding Fibers that have a solid core, and Photonic Bandgap Fibers that have periodic microstructured elements ...
Tutorials
Getting Light into a Monochromator
In this section we give a brief introduction to getting light into a monochromator, and how much you can expect to get out. While the emphasis is on coupling Oriel Light Sources to ...
Tutorials
Polarization in Fiber Optics
A beam of light can be thought of as being composed of two orthogonal electrical vector field components that vary in amplitude and frequency. Polarized light occurs when these two ...
Tutorials
Introduction to Solar Radiation
Radiation from the sun sustains life on earth and determines climate. The energy flow within the sun results in a surface temperature of around 5800 K, so the spectrum of the radiation ...
Tutorials
Introduction to Positioning Equipment
This tutorial introduces opto-mechanical component design basics and will familiarize the reader with the issues that need consideration in the selection of the most commonly used tabletop ...
Tutorials
Calculating Output Power
You can estimate the power in the collimated beams* at any wavelength or in any wavelength range from our Series Q, Apex, or Research Lamp Housings with any of our CW and pulsed arc, ...
Tutorials
Resolution of Monochromators and Spectrographs
Gratings are available in various groove densities (i.e. lines/mm). Higher groove densities give higher reciprocal dispersion and therefore higher resolution. The grating dispersion ...
Tutorials
Fundamentals of Vibration
Vibration and vibration isolation are both intimately connected with the phenomenon of resonance and simple harmonic motion. A simple example of harmonic motion is a mass connected ...
Tutorials
Laws of Radiation
Everything radiates and absorbs electro-magnetic radiation. Many important radiation laws are based on the performance of a perfect steady state emitter called a blackbody or full radiator. ...
Tutorials
How the Picomotor Actuator Works
The Picomotor's actuator relies on the basic difference between dynamic and static friction. A graphic example of this is the “tablecloth trick,” in which a quick pull of the cloth ...
Tutorials
Environmental Vibration Criteria
These generic criterion curves have been developed on the basis of data from individual systems and measurements made in facilities both before and after vibration problems had been ...
Tutorials
Fiber Optic Communication Basics
The theoretical bandwidth of optical fiber transmission in the 1550 nm window alone is on the order of terabits. Current fiber optic systems have not even begun to utilize the enormous ...
Tutorials
Understanding the Compliance Curve
No actual structure is a perfectly rigid body - all structures vibrate by flexing and twisting. The response of structures to random vibrations can be quite complicated because they ...
Page 1 of 2