Page view updated with the selected options.
Technical Notes
Technical Notes
Reliable Spectroradiometry
Reliable spectroradiometry takes a lifetime of work and attention to master. Unreliable spectroradiometry is much easier to accomplish1 all it takes is missing a single critical point, ...
Tutorials
Light Collection and Systems Throughput
This discussion is restricted to the general use of Incoherent Light Sources, such as arc lamp or quartz tungsten halogen sources. Diffraction and coherent effects are excluded. The ...
Selection Guides
Incoherent Light Source Guide
Newport's Oriel® Instruments light source offerings are varied and significant. With so many options, it can be difficult to choose the best system for your application. For light source ...
Technical Notes
Introduction to FTIR Spectroscopy
An FT-IR Spectrometer is an instrument which acquires broadband NIR to FIR spectra. Unlike a dispersive instrument, i.e. grating monochromator or spectrograph, FT-IR Spectrometers collect ...
Tutorials
Getting Light into a Monochromator
In this section we give a brief introduction to getting light into a monochromator, and how much you can expect to get out. While the emphasis is on coupling Oriel Light Sources to ...
Tutorials
Introduction to Solar Radiation
Radiation from the sun sustains life on earth and determines climate. The energy flow within the sun results in a surface temperature of around 5800 K, so the spectrum of the radiation ...
Tutorials
Calculating Output Power
You can estimate the power in the collimated beams* at any wavelength or in any wavelength range from our Series Q, Apex, or Research Lamp Housings with any of our CW and pulsed arc, ...
Tutorials
Resolution of Monochromators and Spectrographs
Gratings are available in various groove densities (i.e. lines/mm). Higher groove densities give higher reciprocal dispersion and therefore higher resolution. The grating dispersion ...
Solution
Oriel Instruments
Oriel products and solutions represent leading instruments, such as light sources covering a broad range from UV to IR, pulsed or continuous, and low to high power.
Technical Notes
Simulation of Solar Irradiation
Oriel® Solar Simulators provide the closest spectral match to solar spectra available from any artificial source. The match is not exact, but better than needed for many applications. ...
Technical Notes
Solar Simulator Standards
A solar simulator is a light source that approximates the illumination of natural sunlight. The ability of a solar simulator to approximate natural sunlight is based on three criteria: ...
Technical Notes
Information on Spectral Irradiance Data
The radiometric data shown at the end of this section was measured in our Standards Laboratory. The wavelength calibrations are based on our spectral calibration lamps. Irradiance data ...
Tutorials
Laws of Radiation
Everything radiates and absorbs electro-magnetic radiation. Many important radiation laws are based on the performance of a perfect steady state emitter called a blackbody or full radiator. ...
Technical Notes
Optical Radiation Terminology and Units
There are many systems of units for optical radiation. In this tutorial, we try to adhere to the internationally agreed CIE system. The CIE system fits well with the SI system of units. ...
Technical Notes
Arc Lamp Spectral Irradiance Data
Spectral irradiance data is shown below for our Arc Lamps. You can click on the curve for a larger image, or on a model number for complete information on a specific arc lamp. Spectral ...
Technical Notes
Optical Detection Systems
In a typical photo-research system, a detector measures the radiant intensity used to evoke photo-response in a sample or the radiant intensity produced by the sample in response to ...
Technical Notes
Oriel® Calibration Light Sources
The most accurate and economical method of wavelength calibration is the spectral calibration lamp. We offer lamps to cover wavelengths from below 185 nm to over 2.5 µm. Be sure to ...
Technical Notes
Solar Simulator Definitions of Characteristics
This glossary briefly defines the terms and units most frequently used in technical discussions around solar simulation.
Technical Notes
Solar Simulator Sample Calculations
The spectral irradiance at any wavelength, Eλ, is in units of watts per square meter per nm (W m-2 nm-1). The value is a measure of the flux per nm at the specified wavelength incident ...
Technical Notes
LEDs Drive the Latest Innovation in Solar Simulator Technology
Newport's PZA Ultra-High Resolution Actuator provides 12.5 mm travel with 50 N load capacity.
Page 1 of 10