Technical Notes
Fundamentals of Spatial Filtering
Spatial filters provide a convenient way to remove random fluctuations from the intensity profile of a laser beam. This greatly improves resolution — which is especially critical for ...
Technical Notes
Polarization Control with Optics
Precise control of polarization behavior is necessary to obtain optimal performance from optical components and systems. Characteristics such as reflectivity, insertion loss, and beamsplitter ...
Technical Notes
UAV Imaging Systems
When equipped with high-performance thermal imaging systems, UAVs, also known as drones, lend themselves to a wide range of defense, government, and commercial applications.
Technical Notes
Beam Expanders
Simple beam expanders are essentially telescopes which, in their most basic forms, consist of two lenses. The input beam is assumed to be collimated. The first lens must have a diameter ...
Technical Notes
Variable Laser Attenuators
Variable laser attenuators consist of essentially two optical components, a half waveplate, and a polarizer with a good extinction ratio, and allow for continuous power control for ...
Technical Notes
Optical Mirror Physics
Optical mirrors consist of metallic or dielectric films deposited directly on a substrate such as glass, differing from common mirrors, which are coated on the back surface of the ...
Technical Notes
Diffraction Grating Physics
A diffraction grating is essentially a multi-slit surface. It provides angular dispersion, i.e., the ability to separate wavelengths based on the angle that they emerge from the gr ...
Technical Notes
Optical Coatings
Optical coatings typically consist of thin films made up of single or multiple layers of either metallic or dielectric materials. When properly designed and fabricated, these coatings ...
Technical Notes
Optical Filter Characteristics
In addition to being deposited on the surface of an optical component, optical coatings can also be incorporated into a single element through deposition on one or many substrates followed ...
Technical Notes
Optical Lens Physics
Lenses are essentially light-controlling elements and so are exploited for light gathering and image formation.
Technical Notes
Fiber Optic Physics
This technical note discusses the fundamental physics of optical fibers, their practical implementation, and the various types of optical fibers.
Technical Notes
Diffraction Grating Part Number System
All standard Richardson gratings have a part number following the format AA BBB CC DD - EEE x
Technical Notes
Focusing and Collimating
As a first example, we look at a common application, the focusing of a laser beam to a small spot. The situation is shown in Figure 5. Here we have a laser beam, with radius y1 and ...
Technical Notes
Gaussian Beam Optics
The Gaussian has no obvious boundaries to give it a characteristic dimension like the diameter of the circular aperture, so the definition of the size of a Gaussian is somewhat arbitrary. ...
Technical Notes
Fiber Optic Coupling
The problem of coupling light into an optical fiber is really two separate problems. In one case, we have the problem of coupling into multimode fibers, where the ray optics of the ...
Technical Notes
Beam Shaping with Cylindrical Lenses
Cylindrical Lenses focus or expand light in one axis only. They can be used to focus light into a thin line in optical metrology, laser scanning, spectroscopic, laser diode, acousto-optic, ...
Technical Notes
Optics Formulas
Light is a transverse electromagnetic wave. The electric E and magnetic M fields are perpendicular to each other and to the propagation vector k, as shown below. Power density is given ...
Technical Notes
Optical Materials
Newport offers a wide variety of spherical and aspherical lenses made from BK 7, UV grade fused silica, Infrared grade Calcium Fluoride (CaF2), Magnesium Fluoride (MgF2), AMTR and Zinc ...
Technical Notes
How to Clean Optics
Dust and stains on Optics can cause scattering, and impurities on the optic surface can react with incident laser light to damage optical coatings. With proper handling and cleaning ...
Technical Notes
Optical Surfaces
The lens application drives the requirements for surface irregularity and surface quality. When preservation of wavefront is critical, λ/4 to λ/8 irregularity should be selected; when ...
Page 1 of 5