Page view updated with the selected options.
Tutorials
Tutorials
Laser Diode Technology
Low-power laser diodes come in a variety of packages. Most have a monitor photodiode integrated with the laser diode. Generally, laser diodes emit light from both ends of their cavity. ...
Solution
ILX Lightwave
ILX Lightwave offers a full line of innovative instruments, test systems and accessories used throughout the world in research and development labs and production areas, wherever photonic ...
Videos
LDC-3916 Multi-channel Modular Laser Diode Controller
The LDC-3916 modular laser diode controller uses interchangeable modules for flexible control options over multiple channels.
Technical Notes
ILX Lightwave Discontinued & Obsolete Products
These discontinued products are no longer sold by ILX Lightwave, but are typically supported for three years from the date on which they were discontinued. Repairs and calibrations ...
Videos
Laser Diode Controller Model LDC-3726
A basic introduction to what LIV measurements are and how to perform them using the LDC-3726’s built-in firmware commands.
Videos
Introduction to the Spartan Laser Diode Production Burn-in System
An introduction to the LTS-7410 Low Power Laser Diode Production Burn-in system and basic functionality of the system
Selection Guides
Laser Diode Mount Guide
ILX Lightwave is the leader in Laser Diode Mounts offering the widest range of high quality precision laser diode mounting fixtures, as well as a complete line of Laser Diode Control ...
Videos
Sentry Reliability and Burn-In Test System
Overview of the ILX Lightwave Sentry bench top laser diode reliability and burn-in test system.
Videos
ReliaTest Software for Laser Diode Test Systems
Our ReliaTest graphical user interface supervisory software allows multiple device types and test scenarios to be easily configured without complicated programming.
Videos
VCSEL Reliability and Burn-In with the LRS-9434
For the fast growing VCSEL market, the Sentinel LRS-9434 and LRS-9434SS systems can be utilized for reliability and burn-in testing, with accompanying probe card fixtures.
Videos
LRS-9434 Fixtures - Probe Card Overview
Probe card fixtures for Newport’s ILX Lightwave LRS-9434 Laser Diode Reliability and Burn-In system allow customers a repeatable and reliable method to probe devices with pad sizes ...
Videos
LDM-4980 Series Laser Diode Mount Setup
Setting up and configuring your Newport ILX Lightwave LDM-4980 series mount for your device.
Videos
LDC-3726 Series Laser Diode Modulation Setup
Modulating a laser diode with the ILX Lightwave LDC-3726 series controller.
Selection Guides
Laser Diode Temperature Controller Guide
Thermoelectric Laser Diode Temperature Controllers are used to control a Thermo-Electric Cooler (TEC) that is typically integrated into a laser diodes package or part of a temperature ...
Manual
OMH-6722B Power Head User's Manual
The OMH-6722B Silicon Power/WaveHead, when coupled to an OMM-6810B Optical Multimeter, provides the capability to accurately measure the power and wavelength of laser sources between ...
Manual
OMH-6732B Power Head User's Manual
The OMH-6732B Short Wavelength Power/WaveHead, when coupled to an OMM-6810B Optical Multimeter, provides the capability to accurately measure the power of laser sources between 350 ...
Application Notes
Testing Bond Quality
There are several methods of testing the quality of the bond, ranging from the destructive, such as a sheer test where the chip is physically broken off its sub-mount, to non-destructive, ...
Application Notes
Using USB Through Virtual COM Ports
The Universal Serial Bus (USB) is quickly replacing GPIB as the accepted communication protocol between the PC and the instrument. While USB lowers the total cost of instrumentation ...
Technical Articles
Specialized Systems Characterize Laser Diodes - Laser Focus World
Device sensitivity to temperature, current, and voltage must be accounted for when designing laser diode test systems.
Manual
TCM-39034 Temperature Controller User's Manual
The TCM-39034 32 Watt Temperature Control Module is a precision TEC control module for use in the LDC-3900 Modular Laser Diode Controller.
Page 1 of 11