Videos

Videos

Picomotor demo using interferometer

A demonstration of the New Focus Picomotor using an interferometer. The Picomotor allows for accurate, minute adjustments that cannot be achieved using a manual micrometer.

Videos

3501 Optical Chopper Setup - New Focus Installation Guide

A step-by-step setup guide for the New Focus 3501 Optical Chopper, including preparation for breadboard mounting. The 3501 Optical Chopper comes with four wheels, a wheel cover, and …

Videos

Using LB1005 Lock Box to lock a Vortex Plus Laser

Learn how to use the LB1005 to lock a Vortex II to a rubidium absorption line in this tutorial. About the LB1005: With a bandwidth of 10 MHz, the Model LB1005 high-speed servo controller …

Videos

GuideStar II Beam Steering Correction System

The GuideStar™ II provides high-reliability high-precision compensation of laser pointing and position drift using two independent New Focus™ Picomotor™ actuated motorized mirror m …

Videos

Laser Interlock - ‪New Focus Installation Guide

Overview demonstration of setting up a New Focus laser, including connection of the interlock required for all new lasers.

Videos

Installing Actuators on a New Focus Stage

A step-by-step guide to installing different types of actuators on a New Focus manual translation stage.

Videos

FAQ: How do I lock/unlock a prism mount?

Learn how to lock or unlock a prism mount by adjusting the leaf spring and vertical pin.

Videos

Setting up a Velocity Laser and Controller

Learn how to setup a Velocity Laser and Controller from New Focus. This video also covers how to change the included 120V fuses for use with 220V.

Videos

3501 Optical Chopper Diagnostic - New Focus Installation Guide

A simple guide for initial diagnostic for a New Focus 3501 Optical Chopper. To view a step by guide for setting up your 3501 chopper visit http://www.youtube.com/watch?v=1EeESvtmPR …

Videos

FAQ: Does the platform of a Lab Jack rotate?

No! See for yourself in this demonstration of New Focus Lab Jacks. Lab Jacks allow precise vertical adjustments, without swapping your posts or optical mounts.

Videos

8742 Picomotor Controller-Driver

The model 8742 is a 4-axis open-loop intelligent motion controller/driver that provides a compact and low cost solution for driving New Focus open-loop Picomotors products.

Videos

Velocity - Front Panel Functions

This video covers the front panel functions for the TLB-6700 controller from New Focus.

Videos

FAQ: Removing a retaining ring from filter wheel

Use a 1/16" or smaller hex key and the opening on each retaining ring to unscrew from a filter wheel.

Videos

New Focus - TLB6800 LN Controller

Setup and operation of the New Focus Vortex Plus and Vantage tunable lasers with the new TLB-6800-LN controller.

Videos

FAQ: Locking optic into claw mount

When using a New Focus Opti-Claw mount, remember to engage the locking screw on the side of the mount.

Videos

Connecting an iPP Intelligent Stepper Motor

The short video shows how to connect the cables to a FC series stage which is equipped with an iPP intelligent stepper motor.

Videos

Vortex Plus Installation Guide

Learn how to setup the new Vortex Plus laser head from New Focus, a Newport Corporation brand.

Videos

9061, 9062 and 9063 Gothic Arch Stages - Reconfiguring Micrometer Location

The actuator mounts on the Gothic Series stages can be easily reconfigured for left-handed operation. The micrometer block is relocated where the push block is and vise versa. The …