Language Selector
Product Comparison

Choose products to compare anywhere you see 'Add to Compare' or 'Compare' options displayed.

Page view updated with the selected options.

Application Notes

Showing 1 - 20 of 33 Application Notes
undefined

Application Notes

Measuring Wide Linewidth Source with OMH-6700

The OMH-6700B series of optical measurement heads measure wavelength to within ±0.5 nm accuracy for the 6730B series and to within ±1 nm for the 6720B series for narrow linewidth sources. ...
undefined

Application Notes

Using a Power Wavehead for Emitter Level Screening of High Power Laser Diode Bars

Emitter level screening has been shown to be an effective tool for testing high power laser diode bars and stacks. Measurement of individual emitter output power, wavelength, and polarization ...
undefined

Application Notes

Calibration and Traceability of ILX Lightwave Optical Power Meters

Traceability refers to an unbroken chain of calibration transfers from a known standard to the instrument in question. At ILX Lightwave, this chain of traceability begins with the primary ...
undefined

Application Notes

Controlling Temperatures of Laser Diodes Thermoelectrically

In many applications, active temperature control improves the performance of optoelectronic devices. In most solid-state detectors, noise decreases with operating temperature. Responsivity ...
undefined

Application Notes

Selecting and Using Thermistors for Temperature Control

Thermally sensitive resistors (thermistors) are used widely in laser diode and detector cooling applications because of their high sensitivity, small size, ruggedness, fast response ...
undefined

Application Notes

Protecting Your Laser Diode

It’s been said that there are two types of researchers - those who have blown a laser diode and those who will. While that may be an exaggeration, it’s certainly true that today’s lab ...
undefined

Application Notes

Laser Diode Characteristics Overview

Diode lasers have been called “wonderful little devices.” They are small and effi cient. They can be directly modulated and tuned. These devices affect us daily with better clarity ...
undefined

Application Notes

Thermistor Calibration and Steinhart-Hart

Thermistors provide an inexpensive and accurate temperature monitor for use with laser diodes. The nonlinear resistancetemperature characteristics of a Negative- Temperature Coeffi ...
undefined

Application Notes

Choosing the Right Laser Diode Mount for Your Application

The multitude of laser diode packages available today make selecting the correct mount for laboratory, development, or production testing seem a daunting task. This Application Note ...
undefined

Application Notes

Mode Hopping in Semiconductor Laser Diodes

In this Application Note, we show that mode hopping is directly correlated to noise in the total intensity, and that this noise is easily detected by a photodiode. We also show that ...
undefined

Application Notes

Pulsing a Laser Diode

Relatively high peak powers and effi cient operation have made pulsed laser diodes ideal for applications such as solid-state laser pumping and range fi nding. These higher peak powers ...
undefined

Application Notes

Optimizing TE Drive Current

This Application Note discusses methods for optimizing the TEC drive current for optimum operation in heating and cooling applications. Thermoelectric coolers (TECs) are widely used ...
undefined

Application Notes

Differences Between Threshold Current Calculations

This application note explains the four Telcorida recognized threshold calculation methods, and why each method will result in a slightly different threshold value.
undefined

Application Notes

Testing Bond Quality

There are several methods of testing the quality of the bond, ranging from the destructive, such as a sheer test where the chip is physically broken off its sub-mount, to non-destructive, ...
undefined

Application Notes

AD590 and LM335 Sensor Calibration

The AD590 is a linear thermal sensor which acts as a constant current source. It produces a current, I, which is directly proportional to absolute temperature, over its useful range ...
undefined

Application Notes

Basic Test Methods for Passive Fiber Components

The ever increasing demand for telecommunications bandwidth is driving the market for the components that make up fi ber-optic networks. This article presents basic principles of passive ...
undefined

Application Notes

PID Control Loops

There are many companies that manufacture temperature controllers with various levels of complexity. These instruments use different algorithms and control loops to maintain set temperature. ...
undefined

Application Notes

High Performance Temperature Control in Laser Diode Test Applications

A typical application in laser diode test is the characterization of laser output over wide temperature ranges, typically from 0°C to 85°C. Quick changes to and rapid stabilization ...
undefined

Application Notes

Modulating Laser Diodes

The external modulation feature found on many ILX Lightwave current sources is a very fl exible circuit that can be used for a wide variety of applications. If the task is to slightly ...
undefined

Application Notes

Laser Diode Burn-In and Reliability Testing

Over 99% of all lasers manufactured in the world today are semiconductor laser diodes. Reliability is a concern in every laser diode application whether it is a simple $10 laser pointer ...
Page 1 of 2