No Results Found
Products Here
Application Notes

Amplitude and Phase Characterization of Ultrashort Laser Pulses

As a consequence of the time-bandwidth uncertainty principle, ultrashort laser pulses carry significant bandwidth. If the spectral components that fall under the bandwidth of the laser …

Application Notes

Fast Steering Mirror Technology Active Beam Stabilization

This note explores dynamic beam stabilization using a fast steering mirror (FSM), a technology originally developed for demanding aerospace pointing and tracking requirements. The performance …

Technical Articles

Optical Mounts: Ignore Them at Your Peril - Photonics Spectra

Optomechanical mounts may seem like insignificant design elements, but they can make or break a photonic application.

Application Notes

Basic Test Methods for Passive Fiber Components

The ever increasing demand for telecommunications bandwidth is driving the market for the components that make up fi ber-optic networks. This article presents basic principles of passive …

Application Notes

Test and Characterization of Laser Diodes

It is often necessary to quantitatively assess the quality, performance, and characteristics of laser diodes. This is done through performing a series of experiments and obtaining certain …

Application Notes

Three-Dimensional Microfabrication by Two-Photon Polymerization

Two-photon polymerization is a serial process for the fabrication of three-dimensional microstructures. Because of its ability to produce geometries with no topological constraints …

Manual

1919-R Optical Power Meter User Manual

The Newport 1919-R is a microprocessor-based Laser Power/Energy Meter that provides a broad range of measurements, displays, and data handling options.

Manual

LDC-37X6 Laser Diode Controller User Manual

The LDC-3706 Laser Controllers are high performance combination current source/temperature controllers. The current source provides a high stability output with a fully redundant current …