Language Selector
Product Comparison

Choose products to compare anywhere you see 'Add to Compare' or 'Compare' options displayed.

Spectrometer Instrumental Bandpass

The instrumental bandpass of an optical spectrometer depends on both the dimensions of the image of the entrance slit and the exit slit dimensions.

Ignoring the effects of the image height, the instrumental bandpass B is given by

B = P sup(w',w")    (8-12)

where P is the reciprocal linear dispersion, w' is the image width, w" is the width of the exit slit, and sup(w',w") is the greater of its arguments:

sup(w',w") = w' if w'>w",  w" otherwise    (8-13)

As P is usually expressed in nm/mm, the widths w' and w" must be expressed in millimeters to obtain the bandpass B in nanometers.

In cases where the image of the entrance slit is wider than the exit slit (that is, w' > w"), the instrumental bandpass is said to be imaging limited, whereas in those cases where the exit slit is wider than the image of the entrance slit (w' < w"), the instrumental bandpass is said to be slit limited. [When an imaging-limited optical system is imaging limited due primarily to the grating, either because of the resolving power of the grating or due to its wavefront errors, the system is said to be grating limited.]

Figure 8-10. Effect of exit slit height on image width. Both the width and the height of the image are reduced by the exit slit chosen. Even if the width of the exit slit is greater than the width of the image, truncating the height of the image yields w'* < w'. [Only the top half of each image is shown.]

In the design of optical spectrometers, the widths of the entrance and exit slits are chosen by balancing spectral resolution (which improves as the slits become narrower, to a limit) and optical throughput (which improves as the slits widen, up to a limit). Ideally, the exit slit width is matched to the width of the image of the entrance slit  – this optimizes both resolution and throughput. This optimum may only be achievable for one wavelength, the resolution of the other wavelengths generally being either slit-limited or imaging-limited (with suboptimal throughput likely as well).


Diffraction Gratings Handbook Cover

For footnotes and additional insights into diffraction grating topics like this one, download our free MKS Diffraction Gratings Handbook (8th Edition)

Download a Handbook