Efficiency Characteristics of Diffraction Gratings

Efficiency and its variation with wavelength and spectral order are important characteristics of a diffraction grating. For a reflection grating, efficiency is defined as the energy flow (power) of monochromatic light diffracted into the order being measured, relative either to the energy flow of the incident light (absolute efficiency) or to the energy flow of specular reflection from a polished mirror substrate coated with the same material (relative efficiency). [Intensity may substitute for energy flow in these definitions.] Efficiency is defined similarly for transmission gratings, except that an uncoated substrate is used in the measurement of relative efficiency.

High-efficiency gratings are desirable for several reasons. A grating with high efficiency is more useful than one with lower efficiency in measuring weak transition lines in optical spectra. A grating with high efficiency may allow the reflectivity and transmissivity specifications for the other components in the spectrometer to be relaxed. Moreover, higher diffracted energy may imply lower instrumental stray light due to other diffracted orders, as the total energy flow for a given wavelength leaving the grating is conserved (being equal to the energy flow incident on it minus any scattering and absorption).

Control over the magnitude and variation of diffracted energy with wavelength is called blazing, and it involves the manipulation of the micro-geometry of the grating grooves. As early as 1874, Lord Rayleigh recognized that the energy flow distribution (by wavelength) of a diffraction grating could be altered by modifying the shape of the grating grooves.84 It was not until four decades later that R.W. Wood showed this to be true when he ruled a grating on which he had controlled the groove shape, thereby producing the first deliberately blazed diffraction grating.

The choice of an optimal efficiency curve for a grating depends on the specific application. For some cases the desired instrumental response is linear with wavelength; that is, the ratio of intensity of light and the electronic signal into which it is transformed is to be nearly constant across the spectrum. To approach this as closely as possible, the spectral emissivity of the light source and the spectral response of the detector should be considered, from which the desired grating efficiency curve can be derived. Usually this requires peak grating efficiency in the region of the spectrum where the detectors are least sensitive; for example, a visible-light spectrometer using a silicon detector would be much less sensitive in the blue than in the red, suggesting that the grating itself be blazed to yield a peak efficiency in the blue.

A typical efficiency curve (a plot of absolute or relative diffracted efficiency vs. diffracted wavelength λ) is shown in Figure 9-1. Usually such a curve shows a single maximum, at the peak wavelength (or blaze wavelength) λB. This curve corresponds to a given diffraction order m; the peak of the curve decreases in magnitude and shifts toward shorter wavelengths as |m| increases. The efficiency curve also depends on the angles of use (i.e., the angles of incidence and diffraction). Moreover, the curve depends on the groove spacing d (more appropriately, on the di-mensionless parameter λ/d) and the material with which the grating is coated (for reflection gratings) or made (for transmission gratings).

Figure 9-1. A typical (simplified) efficiency curve. This curve shows the efficiency E of a grating in a given spectral order m, measured vs. the diffracted wavelength λ. The peak efficiency EP occurs at the blaze wavelength λB.

In many instances the diffracted power depends on the polarization of the incident light. P-plane or TE polarized light is polarized parallel to the grating grooves, while S-plane or TM polarized light is polarized perpendicular to the grating grooves (see Figure 9-2). For completely unpolarized incident light, the efficiency curve will be exactly halfway between the P and S efficiency curves.

Figure 9-2. S and P polarizations. The P polarization components of the incident and diffracted beams are polarized parallel to the grating grooves; the S components are polarized perpendicular to the P components. Both the S and P components are perpen-dicular to the propagation directions.

Usually light from a single spectral order m is used in a spectroscopic instrument, so a grating with ideal efficiency characteristics would diffract all the power incident on it into this order (for the wavelength range considered). In practice, this is never true: the distribution of the power by the grating depends in a complicated way on the groove spacing and profile, the spectral order, the wavelength, and the grating material.

Anomalies are locations on an efficiency curve (efficiency plotted vs. wavelength) at which the efficiency changes abruptly. First observed by R. W. Wood, these sharp peaks and troughs in an efficiency curve are sometimes referred to as Wood's anomalies. Anomalies are rarely observed in P polarization efficiency curves, but they are often seen in S polarization curves (see Figure 9-3).

Figure 9-3. Anomalies in the first order for a typical grating with triangular grooves. The P efficiency curve (solid line) is smooth, but anomalies are evident in the S curve (dashed line). The passing-off locations are identified by their spectral order at the top of the figure.

Diffraction Gratings Handbook Cover

For footnotes and additional insights into diffraction grating topics like this one, download our free MKS Diffraction Gratings Handbook (8th Edition)

Download a Handbook