Once a lamp has been turned on or ignited, it is beneficial the lamp's health to keep the lamp on instead of frequently turning the lamp on and off. Oriel® external shutters provide a convenient method of blocking the light output of a lamp while a test fixture is being set up or adjusted.
- Useful for radiometric zeroing of photodetector
- Reduce number of lamp starts or ignitions required
- Manual/TTL control shutter option
- Electronic Safety Shutter capable of external control, contact closure See All Features
Features
Manual/TTL Shutter Option
Electronic Safety Shutter Capable of External Control, Contact Closure
Reduce Number of Lamp Starts or Ignitions Required
Many optical applications require the use of broadband light sources such as our arc or QTH lamps. However, often during the setup or testing phases of an experiment the lamp’s light is not necessary as it could be damaging to the user or sample under test. Frequently igniting the lamp or toggling its power supply are not practical solutions for blocking the light as these actions cause added strain and can drastically reduce the lamp’s lifetime. Instead, these low light leakage shutters offer a simple solution to blocking the output path of a lamp housing when light output is not needed. These shutters can be used to allow the lamp to warm-up while the user configures their equipment, let the user make minor adjustments to the setup throughout testing, or permit the user to change samples under test all without disturbing the lamp’s internal function. When using arc lamps, these shutters are recommended to block the user or sample from unnecessary UV radiation exposure.
Useful for Radiometric Zeroing of a Photodetector
Radiometric zeroing is the process of defining a negative offset when light is not incident on a photodetector. This process is used in practice to filter background noise from the detector and associated electronics when taking light measurements. These low light leakage shutters offer a simple way to "zero" a photodetector.
Accessories
Lamp Housings
| Compare | Description | Drawings, CAD & Specs | Avail. | Price | ||
|---|---|---|---|---|---|---|
![]() | 60000Lamp Housing, Q Series, Adjustable Reflectors & Up to 4 Condensers | In Stock | ||||
![]() | 66901Arc Lamp Housing, Research, 50-500 W, F/1.5 Plano-Convex, 1.5 Inch Flange | In Stock | ||||
![]() | 66885QTH Lamp Housing, Research, 600-1000 W, F/1, 2 Element FS, Collimated | In Stock | ||||
![]() | 66881QTH Lamp Housing, Research, 10-250 W, F/0.85 Borofloat Glass, Collimated | In Stock | ||||
![]() | 66902Arc Lamp Housing, Research, 50-500 W, F/1 2 Element Plano-Convex, 1.5 Inch Flange | In Stock | ||||
![]() | 67001Arc Lamp Housing, Research, 50-500 W, F/2.2 Asphere, 1.5 Inch Flange | In Stock | ||||
![]() | 66921Arc Lamp Housing, Research, 450-1000 W, F/1 2 Element Plano-Convex, 2 Inch Flange | 2 Weeks | ||||
![]() | 66923Arc Lamp Housing, Research, 450-1000 W, F/0.7, 4 Element Aspherab, 3 Inch Flange | In Stock | ||||
![]() | 67011QTH Lamp Housing, Research, 10-250 W, F/1 FS Asphere, Collimated | 4 Weeks | ||||
![]() | 67009QTH Lamp Housing, Research, 10-250 W, F/2.2 FS Asphere, Collimated | 3 Weeks | ||||
![]() | 67005Arc Lamp Housing, Research, 50-500 W, F/1 Asphere, 1.5 Inch Flange | In Stock |