Show Filters:
Showing 6 of 6 total products
Compatibility:
Compare Description Drawings, CAD & Specs Lamp WattageLamp TypeCondenser TypeFlange Series SizeF/# Avail. Price
High Power Mercury-Xenon Light Sources66926-500HX-R07500 WHg(Xe)Four Element Aspherab3 InchF/0.7
$16,390
High Power Mercury-Xenon Light Sources66924-500HX-R1500 WHg(Xe)Two Element Plano-Convex2 InchF/1
$14,735
High Power Mercury-Xenon Light Sources66926-1000HX-R071000 WHg(Xe)Four Element Aspherab3 InchF/0.7
$16,075
High Power Mercury-Xenon Light Sources66924-1000HX-R11000 WHg(Xe)Two Element Plano-Convex2 InchF/1
$13,910
High Power Mercury-Xenon Light Sources66926-1000HXF-R071000 WHg(Xe), Ozone FreeFour Element Aspherab3 InchF/0.7
$17,930
High Power Mercury-Xenon Light Sources66924-1000HXF-R11000 WHg(Xe), Ozone FreeTwo Element Plano-Convex2 InchF/1
$13,910

Specifications

  • Type
    Mercury-Xenon Light Source
  • Output Beam
    Collimated
  • Lens Material
    Fused Silica
  • Lens Transmittance Range
    200 - 2500 nm
  • Light Ripple
    <1 % rms
  • Power Requirements
    95 - 264 VAC

Features

All Necessary Components for Lamp Operation Included

High power research light sources includes an arc lamp, appropriate socket adapter, lamp housing interconnection cables, power supply, and Research lamp housing. After a quick and easy assembly, the light source is ready for use and easily integrated into a user's setup. The lamp housings offered with these light source kits are capable of operating all 450-1000 W DC arc lamps. This allows the user to interchange lamps in their setup simply by replacing the lamp and socket adapter (if necessary) in their lamp housing.

Simple Lamp Alignment Process

Due to small manufacturing differences between lamps, the rear reflector position and lamp position relative to the condenser lens must be adjusted when a new lamp is installed in the housing. Adjustment knobs located on the exterior of the lamp housing allow for optimum positioning of the lamp and rear reflector.

High Power Mercury-Xenon Hg(Xe) Lamps

Hg(Xe) arc lamps include a mixture of mercury and xenon gas, with the mixture of mercury giving the lamp a higher output intensity and pronounced spectral emission lines in the UV and visible spectrum. Applications requiring higher intensity and sharper emission lines in the UV to visible such as film thickness measurement and UV curing take advantage of these unique characteristics.

  • : 500 W Hg(Xe) Lamp
  • : 1000 W Hg(Xe) Lamp
  • : 1000 W Hg(Xe) Lamp, Ozone Free

High Stability Arc Lamp Power Supply

The  power supply provided with these light sources is a highly regulated power supply. Much of an arc lamp's stability in wavelength and output intensity is due to keeping the temperature and pressure of the gas inside the lamp's envelope as constant possible. The 69920 power supply provides highly stable voltage and current supply to the arc lamp, keeping the arc lamp's ripple to less than 1% rms while maximizing the lifetime of the lamp.

High Power Research Lamp Housing

Oriel's Research Lamp Housings are designed to focus the output light of the lamp to the user's needs while providing an ideal environment for lamp operation and user safety. A built in temperature sensor and cooling fan prevents overheating of the lamp during operation. A rear reflector built inside the lamp housing reflects back scatter radiation from the lamp. The collimating lens assembly on each Research Lamp Housing is used to ensure the lamp is properly aligned within the housing and optimally focus the light output to the user’s needs. If the lamp housing door is not firmly secured to the lamp housing or a lamp housing interconnection cable is not firmly secured to its connector, the lamp inside will not ignite or supply voltage and current to the lamp will not be supplied. This protects the user from accidental exposure to UV radiation and high voltage during ignition and operation of the lamp.

Two Condenser Lens Options

Lamp Housing with Two Element Plano-Convex Condenser Lens

Light sources with a -R1 suffix include the model high power research lamp housing. This housing has a 2 Inch series flange series and offers 48 mm diameter, collimated light output. The condenser lens included is a F/1 two-element plano-convex lens with the secondary lens in place to correct spherical aberration from the first.

Light sources with a -R07 suffix include the model high power research lamp housing. This housing has a 3 Inch flange series and a 69 mm diameter, collimated light output. The condenser lens contains a F/0.7 four element Aspherab™ lens assembly, the most efficient light collection setup offered that is almost free of spherical aberration.

Arc Lamp Safety

Arc lamps may emit dangerous levels of UV radiation depending on their source type. Ensure that only authorized personnel are in the vicinity of the source, and wearing the necessary safety equipment such as UV protective eyewear, clothing, and gloves. Lighted UV warning signs, posted outside laboratory doors where UV sources are operating, can prevent accidental exposure. Newport also recommends using an electronic shutter to block the beam when the source is not in use but remains turned on. Alternatively, the beam can be safely contained by using beam tubes or fiber optic cables to deliver the light to a sample. It is recommended to vent the ozone that is produced by some lamp models to the outside or use the

Accessories

Safety Equipment

Compare Description Drawings, CAD & Specs Avail. Price
49121Ultraviolet Protective Gloves, Size 10, Black Neoprene, Set of 3
$75
49123UV Protective Gloves, Size 8, Black Neoprene, Set of 3
$75
49126Safety Goggles, UV Light Sources, Flexible Frame
$80
66087Ozone Eater™, 110/220 VAC, 50/60 Hz$2,090