Compare Model Drawings, CAD & Specs Lamp Wattage Flange Series Size F/# Condenser Type Availability Price
$3,705
50 - 500 W 1.5 Inch F/1 Two Element Plano-Convex
$3,855
50 - 500 W 1.5 Inch F/1 Asphere
$3,600
50 - 500 W 1.5 Inch F/1.5 Plano-Convex
$3,800
50 - 500 W 1.5 Inch F/2.2 Asphere
$5,515
450 - 1000 W 2 Inch F/1 Two Element Plano-Convex
$9,785
450 - 1000 W 3 Inch F/0.7 Four Element Aspherab

Specifications

  • Type
    Arc Lamp Housing
  • Lamp Type
    Xenon, Mercury, Mercury-Xenon
  • Output Beam
    Collimated
  • Lens Material
    Fused Silica
  • Lens Transmittance Range
    200 - 2500 nm

Features

Rear Reflector for Increased Light Output

A rear reflector is built into the lamp housing to collect back scatter from the lamp that would otherwise be lost. An estimated 60% increase in output intensity from the lamp housing is observed due to this rear reflector. Due to small manufacturing differences between lamps, the rear reflector needs to be adjusted when a new lamp is installed.

Simple Lamp Alignment Process

Due to small manufacturing differences between lamps, the rear reflector position and lamp position relative to the condenser lens must be adjusted when a new lamp is installed in the housing. Adjustment knobs located on the exterior of the lamp housing allow for optimum positioning of the lamp and rear reflector.

Integrated Lamp Cooling Fan and Safety Interlock Feature

A temperature sensor inside the lamp housing monitors the lamp's operating temperature and controls the cooling fan accordingly. This keeps the lamp at a safe temperature for operation and ensures the temperature required for proper wavelength emission of the lamp is maintained. The Research Lamp Housing also includes as Safety Interlock Feature. If the lamp housing door or interconnection cable to the power supply are not firmly secured, the lamp will not ignite or voltage supply to the lamp will cease. This protects the user from accidental exposure to UV radiation and high voltage.

Built-in Ignitor

Starting an arc lamp requires a pulse ranging from several hundred to several thousands of volts to excite the gas between the lamp's electrodes. An ignitor is built into the lamp housing to meet this requirement.

Three Different Flange Sizes Available

Output flanges of 1.5 inches, 2 inches, and 3 inches are coupled to the output of these Research Lamp Housings. The output flange size determines the diameter of the collimated output beam and should also be considered based on what component the lamp housing will be coupled to. Flange couplers and adaptors for interchanging between different flange sizes are offered if this is required to couple the lamp housing to a monochromator or other piece of equipment.

Interchangeable Lamps

Oriel® offers Research Lamp Housings capable of operating two different ranges of lamp wattages: 50 to 500 W and 450 to 1000 W. All Xenon, Mercury-Xenon, and Mercury arc lamps can be operated in the lamp housing that matches their lamp wattage. The appropriate socket adapter, Lamp Housing Interconnection Cable, and Arc Lamp Power Supply is also necessary to operate the lamp. Check out the Compatibility guide below for more information.

Three Different Lens Types Used

Oriel uses three different types of lenses to use in Condenser Lens configurations. These lens types differ in cost and quality of output beam collimation quality:

  • Plano Convex: Most economic lens option, utilizes an asymmetric lens shape to minimize spherical aberration
  • Aspheric: The front surface of an aspheric lens gradually changes in curvature from the center of the lens to the edge. This shape reduces spherical aberration more effectively than a Plano Convex Lens
  • Aspherab™: This lens configuration provides the highest quality output light. Four different lenses are used in a unique configuration to provide light output that is nearly free from spherical aberration.
Condenser lens assemblies also differ in f/#. A smaller f/# means the lens is placed closer to the light source inside the lamp housing. This allows for greater radiant flux as more light is collected by the lens. However, this also causes greater lens aberration. As a result, more light does not mean more quality light. Higher f/#'s are suggested if a high quality collimated beam is needed from the output of the lamp housing. However, lower f/#'s are suggested for coupling to a monochromator due to their higher throughput. The output wavelength required from the lamp should also be considered when choosing a lamp housing.

Arc Lamp Safety

Arc lamps may emit dangerous levels of UV radiation depending on their source type. Ensure that only authorized personnel are in the vicinity of the source, and wearing the necessary safety equipment such as UV protective eyewear, clothing, and gloves. Lighted UV warning signs, posted outside laboratory doors where UV sources are operating, can prevent accidental exposure. Newport also recommends using an electronic shutter to block the beam when the source is not in use but remains turned on. Alternatively, the beam can be safely contained by using beam tubes or fiber optic cables to deliver the light to a sample. It is recommended to vent the ozone that is produced by some lamp models to the outside or use an Ozone Eater.

Compatibility

Light Source Components Compatible with 50 - 500 W Research Arc Lamp Housings

Lamp Type Lamp Model Lamp Socket Adapter Power Supply Cable Complete System 
 Xenon 6251NS 66150 69907 70050  Low Power Xe
6263
6257
6255 66151
6254
6256 66152 69907 70050 -
6259 66160 69911 70050 Medium Power Xe
6258
Mercury 6282 66158 69907 70051 Low Power Hg
6281 66150 69907 70051 -
6283NS 66144 69910 70051 Medium Power Hg
6286 66161
6285 66162
Mercury-Xenon 6290 66169 69911 70050 Medium Power Hg-Xe
6291 66152
66142 66159

Light Source Components Compatible with 450 - 1000 W Research Arc Lamp Housings

Lamp Type Lamp Model Lamp Socket Adapter Power Supply Cable Complete System 
Xenon 6279NS 6163 69920 70052* High Power Xe
6278
6271 6162
6269
Mercury-Xenon 66142 6379 69920 70052* High Power Hg-Xe
6293 6162
6295NS
*70052 cable set is included in 69921 and 69923 housing.