Technical Notes

Technical Notes

ILX Lightwave Discontinued & Obsolete Products

These discontinued products are no longer sold by ILX Lightwave, but are typically supported for three years from the date on which they were discontinued. Repairs and calibrations …

Technical Notes

Repeatability of Wavelength and Power Measurements Using the OMM-6810B

This technical note presents the experimental results showing the repeatability of power and wavelength measurements using the OMM-6810B Optical Power and Wavelength Meter coupled to …

Technical Notes

LDX-3232 Modulation Bandwidth

This Tech Note provides information on the modulcation bandwidth of the LDX-3232 High Compliance Laser Diode Driver. The output of the LDX-3232 is capable of being modulated via a signal …

Technical Notes

Typical Output Stability of the LDX-3100 Board Level Current Source

This technical note presents the results of output drift measurement tests performed on a typical LDX-3100 Board-Level Precision Current Source.

Technical Notes

Square Wave Modulation of the LDX-3500B

The ILX Lightwave LDX-3500B Series Precision Current Source can be modulated by an external analog signal up to 500 kHz, 150 kHz or 100 kHz depending on the model.

Technical Notes

Typical Output Noise of an LDX-3412

This technical note presents the results of noise measurements made on a typical production run of LDX-3412 Precision Current Sources.

Technical Notes

Typical Output Drift of an LDX-3412

The measurement setup is shown in Figure 1. Each LDX-3412 was placed in a temperature controlled oven and stabilized for one hour at 25oC. Current measurements were taken by measuring …

Technical Notes

Long-Term Output Stability of an LDX-3525B

The measurement setup is shown in Figure 1. The LDX-3525B was placed in a temperature controlled oven and stabilized for one hour at 20oC. The LDX-3525B was placed in low (200 mA) range, …

Technical Notes

Output Current Accuracy of an LDX-3525B

This technical note presents the results of measurement (display) accuracy tests performed on a typical production model LDX-3525B Precision Current Source.

Technical Notes

LDX-36000 QCW Pulse Characteristics

The LDX-36000 series High Power Current Source is a versatile instrument that can function in both continuous-wave (CW) and quasicontinuous-wave (QCW) modes.

Technical Notes

Clamping Limit of an LDX-3525B

The measurement setup is shown in Figure 1. Each tested unit was set to drive a 1W load, with the DC output level set to 100 mA, and the limit set at 125 mA. The output was then modulated …

Technical Notes

Facility Power Requirements for the LDX-36000

This Tech Note details the input power requirements of the ILX Lightwave LDX-36000 series high power laser diode drivers.

Technical Notes

Using the Dual Modulation Inputs of the LDX-3620B

The LDX-3620B is an ultra-low noise, high stability current source with two external modulation inputs. This technical note describes the use of the dual modulation inputs of the L …

Technical Notes

Effects of Cabling and Inductance When Pulsing High Power Laser Diodes

This technical note discusses the effects of inductance when pulsing high power laser diodes with high current. It also discusses cabling and connections between the current source …

Technical Notes

Long-Term Output Stability of the LDX-3620B

This technical note presents the results of output drift measurements performed on a typical production model LDX-3620B Ultra-Low Noise Laser Diode Current Source.

Technical Notes

LDC-3736 Laser Protection

The LDC-3736 Quantum Cascade Laser Controller is designed to safely drive quantum cascade lasers (QCLs) with up to 4 Amps of current and a compliance voltage of 18 Volts.

Technical Notes

Broadband Noise Measurements for Laser Diode Current Sources

This technical note describes the measurement of broadband noise found in laser diode current sources. A description of the test setup is presented with the results shown in graphical …

Technical Notes

Quick Start: Modulating a Laser Diode Driver

Most ILX Lightwave laser diode current sources and controllers have an external modulation input. This technical note gives a quick overview on setting up an ILX Lightwave laser diode …

Technical Notes

Typical Output Stability of the LDC-3724B

The test was performed with the 3724 and the test loads inside an environmental chamber set to 25°C ± 0.5°C. The test load used to measure laser drive current stability consisted of …

Technical Notes

Using Status Event Registers for Event Monitoring

When using GPIB to perform automated tests or experiments the user may want to know when specific events occur. This can be done by continually polling an instrument using software …

Page 1 of 5