Technical Notes

Technical Notes

Fundamentals of Spatial Filtering

Spatial filters provide a convenient way to remove random fluctuations from the intensity profile of a laser beam. This greatly improves resolution — which is especially critical for …

Technical Notes

Laser Diode Production Burn-In

High temperature burn-in screening is used in laser diode manufacturing to screen out devices that are likely to have unacceptably short lives and to ensure that the remaining population …

Technical Notes

Laser Diode Life Testing

Life test studies are used to collect laser diode lifetime data under carefully controlled operating conditions. These data are then used to develop statistical models that can predict …

Technical Notes

Laser Diode Characterization

Laser diodes are characterized by their inherent physical properties within five distinct categories, including: electrical, spatial, spectral, optical, and dynamic properties.

Technical Notes

Optical Transceiver Physics

OE converters typically employ photodiodes to absorb incoming photons and convert them into electrical current. Photodiodes are devices in which p-type, n-type, and intrinsic semiconductors …

Technical Notes

Optical Fiber Alignment

Good fiber alignment produces the highest coupling efficiency and therefore the least signal loss before assembly or packaging of an optical system.

Technical Notes

Solar Light Simulation

The surface temperature of the sun is approximately 5800 K; this means that the electromagnetic spectrum of radiation from the sun is similar to that of a 5800 K blackbody with the …

Technical Notes

Tunable Incoherent Light Sources

The TLS is versatile, being both a broadband and high-resolution monochromatic light source which makes it suitable for applications such as the study of wavelength-dependent chemical …

Technical Notes

Designing with VIB320 Vibration Isolation Bearings

Newport's VIB320 Series isolators utilize patented VIBe™ technology to attenuate the transmission of vibrations without the need for electronics, air hoses, compressor or other supporting …

Technical Notes

Essentials of Laser Safety

Learn about laser classifications and the controls and protective equipment required to stay safe.

Technical Notes

Diffraction Grating Part Number System

All standard Richardson gratings have a part number following the format AA BBB CC DD - EEE x

Technical Notes

Reliable Spectroradiometry

Reliable spectroradiometry takes a lifetime of work and attention to master. Unreliable spectroradiometry is much easier to accomplish1 all it takes is missing a single critical point, …

Technical Notes

Fundamentals of Laser Diode Control

To assess the quality, performance, and characteristics of laser diodes, manufacturers often perform exhaustive testing which requires electro-optical, spectral and spatial characterization …

Technical Notes

Thermopile Sensor Physics

Thermopile sensors are based on thermocouples. A thermocouple consists of two dissimilar metals connected in series. To detect radiation, one metal junction is typically blackened to …

Technical Notes

Pyroelectric Sensor Physics

A pyroelectric crystalline material has electric polarization even in the absence of an applied voltage. On heating, the material expands and produces a change in the polarization which …

Technical Notes

Photodiode Sensor Physics

A photodiode sensor consists of a semiconductor p-n junction. Light falling on the junction causes the formation of electron-hole pairs. In photovoltaic mode, the electron-hole pairs …

Technical Notes

Polarization Control with Optics

Precise control of polarization behavior is necessary to obtain optimal performance from optical components and systems. Characteristics such as reflectivity, insertion loss, and beamsplitter …

Technical Notes

UAV Imaging Systems

When equipped with high-performance thermal imaging systems, UAVs, also known as drones, lend themselves to a wide range of defense, government, and commercial applications.

Technical Notes

Laser Physics

A laser is a source of coherent light. It contains an optical oscillator that increases the amplitude of an optical field while maintaining its phase. This coherent amplification is …

Technical Notes

Light-Matter Interactions in Lasers

Light is generated from a laser as a result of the following process: electrons in a material move from an excited energy level to a lower-lying energy level and produce photons that …

Page 1 of 18