Suggested Categories

Showing 1226 products in 129 families
Products Here
Technical Notes

Stage and Controller Compatibility Guide

The following table lists all Newport positioners and the compatible Newport motion controllers and or driver card. Most stages feature ESP technology that provides true plug and …

Selection Guides

Dichroic Filter Guide

Dichroic filters separate a broad spectrum of light into two components: a reflected component and a transmitted component. They provide the ability to select different bands from a …

Videos

LRS-9434 Fixtures - Probe Card Overview

Probe card fixtures for Newport’s ILX Lightwave LRS-9434 Laser Diode Reliability and Burn-In system allow customers a repeatable and reliable method to probe devices with pad sizes …

Manual

XPS-DRV00/XPS-DRV00P Pass Through Driver Card Information

XPS-DRV00P is a pass through board. It is an interconnect board for external amplifiers connected to the XPS controller developed for the new CIE05 board and requires firmware version …

Technical Notes

Fiber Optic Coupling

The problem of coupling light into an optical fiber is really two separate problems. In one case, we have the problem of coupling into multimode fibers, where the ray optics of the …

Tutorials

Optical Power Measurement

When a photon hits the photodiode material, it may generate an electron-hole pair depending on the quantum efficiency of the device. Quantum efficiency is dependent on many factors, …

Solution

ILX Lightwave

ILX Lightwave offers a full line of innovative instruments, test systems and accessories used throughout the world in research and development labs and production areas, wherever photonic …

Technical Notes

Newport ESP Technology

Newport controllers automatically configure ESP-compatible stages delivering true Plug-and-Play for a quick and safe start to positioning applications. Newport's ESP (Enhanced System …

Videos

VCSEL Reliability and Burn-In with the LRS-9434

For the fast growing VCSEL market, the Sentinel LRS-9434 and LRS-9434SS systems can be utilized for reliability and burn-in testing, with accompanying probe card fixtures.

Selection Guides

Motorized Optical Mount Guide

Motorized optical mounts are great for automating sensitive lab or production optical systems, as well as making adjustments in tight spaces where manual adjustment is not possible …

Selection Guides

Balanced Photoreceiver Guide

A balanced photoreceiver consists of two well-matched photodetectors so that a small signal not subtracted is amplified. Balanced Photoreceivers are especially useful in applications …

Videos

USFW-100 Universal Filter Wheel

Oriel’s USFW-100 Universal Standalone Filter Wheel is an excellent choice where a standalone filter wheel or direct drop-in replacement for any previous model Oriel filter wheels is …

Selection Guides

Aspherical Lens Guide

Choosing the right lens shape is critical in order to minimize the optical aberrations. Multiple lenses can be used where one singlet can cancel the aberration caused by another. Generally, …

Application Notes

Workstation for Laser Direct-Write Processing

Lasers exhibit a number of features that makes them unique sources of energy for several material processing methods. For example, they are indispensable tools for drilling, welding, …

Application Notes

AWARE - Wide Field of View Camera

Recent advances in imaging technology coupled with an increasing demand in defense and security control have made it possible to deploy camera sensors in target tracking applications …

Technical Notes

Using Three-Wire RTDs with the LDT-5900 Series

Three-wire RTD temperature sensors are commonly used in applications where the RTD is located a substantial distance from the temperature controller. Three-wire RTDs can be configured …

Technical Notes

LRS-9424 Heat Sink Temperature Stability When Chamber Door is Opened and Closed

This technical note presents the results of tests where the LRS-9424 chamber door is opened and closed while fixtures are operating at different temperature set points.

Technical Notes

LRS-9424B Transient Protection

Protection from harmful electrical transients is important in all applications of laser diodes due to the highly sensitive nature of these semiconductor devices. This is particularly …

Technical Notes

Voltage Drop Across High Current TEC Interconnect Cables

This ILX Lightwave Technical Note compares the voltage drop across the standard and high-current interconnect cables available from ILX Lightwave, and identifies where each cable should …

Manual

XPS-DRVP1 Driver Board User's Manual

The XPS-DRVP1 is an XPS compatible driver card that can drive piezo-stack based NanoPositioning products, with model numbers that end with a '–D'.