Product Comparison

Choose products to compare anywhere you see 'Add to Compare' or 'Compare' options displayed.

Page view updated with the selected options.

Technical Notes

Showing 1 - 20 of 183 Solutions
undefined

Solution

Lithium-Ion Battery Manufacturing Solutions

The global demand for lithium-ion batteries has been growing for a number of years, and this growth isn’t going to stop. Laser manufacturing enables next-generation battery designs ...
undefined

Application Notes

Ophthalmic Surgery

Ophthalmology is the branch of medicine that deals with the anatomy, physiology and diseases of the eye. The laser is particularly suited to ophthalmic surgery since it can provide ...
undefined

Application Notes

Super-Resolution Microscopy (STED and PALM)

One super-resolution approach is called stimulated emission depletion (STED) microscopy. This technique uses a confocal microscope and a diffraction limited excitation beam that is ...
undefined

Application Notes

PCB Manufacturing

Lasers are routinely used in a variety of PCB manufacturing processes including via drilling, depaneling, profiling, laser direct imaging, repair, trimming, and marking. Laser processing ...
undefined

Application Notes

Solar Panel Manufacturing

Crystalline-Silicon solar cells are the predominant solar cell technology used in fabricating solar panels because of the availability of silicon, well-developed manufacturing processes, ...
undefined

Application Notes

Semiconductor Inspection

In this application note, we provide a brief description of the basics of wafer and reticle inspection techniques and discuss the characteristics of current inspection tools.
undefined

Application Notes

Semiconductor Lithography Overview

Lithography is defined as "a method of printing from a flat surface (such as a smooth stone or a metal plate) that has been prepared so that the ink will only stick to the design that ...
undefined

Application Notes

Semiconductor Manufacturing Overview

This application note provides a brief overview of semiconductor manufacturing and describe the various optical techniques used to define, inspect, and measure feature sizes and layer ...
undefined

Application Notes

Real-Time Laser Power Measurement

Only when performing optimally can laser systems guarantee the most cost-effective production of high-quality components. Even the smallest deviations in beam adjustment or focal position ...
undefined

Application Notes

Thermal Imaging

Thermal imaging techniques involve discriminating between various objects in a scene based on their respective differences in temperature.
undefined

Application Notes

Photoacoustic Microscopy (PAM)

Unlike the pure optical microscopy techniques, PAM takes advantage of the weak acoustic scattering in tissue and thus breaks through the optical depth penetration limit (~ 1 mm) in ...
undefined

Application Notes

Two-Photon Fluorescence Microscopy (2PF)

In 2PF, two photons are simultaneously absorbed to cause a higher energy electronic transition in a fluorescent molecule.
undefined

Application Notes

Three-Photon Fluorescence Microscopy (3PF)

Three-photon fluorescence (3PF) microscopy can provide a significant advantage over 2PF microscopy in strongly scattering samples such as the mouse brain.
undefined

Application Notes

Raman Spectroscopy (CARS and SRS)

In CARS microscopy, the pump and Stokes beams are tightly focused into the sample and a CARS image is generated by scanning either the sample or the laser beams.
undefined

Application Notes

Optogenetics

Optogenetics combines genetic and optical techniques to selectively and specifically modulate signaling pathways in intact living organisms using light.
undefined

Solution

Quantum Technology Research Solutions

For over 50 years, MKS has provided components and expertise for thousands of systems and optical applications in a variety of markets. We offer a full range of products for quantum ...
undefined

Solution

Photonics Solutions for Semiconductor Manufacturing

MKS is more than just a provider of great products for semiconductor manufacturing. We are your partner who can provide the solutions you need to help meet the current and future semiconductor ...
undefined

Application Notes

Powder Bed Fusion

Powder bed fusion systems utilize a heat source—such as a laser—to sinter or melt ultra-fine layers of material like powdered metal to fuse into the desired shape.
undefined

Application Notes

Vat Polymerization

In vat polymerization systems—including stereolithography (SLA) and digital light processing (DLP)—a UV laser constructs an object in a vat of a liquid photopolymer resin by curing ...
undefined

Application Notes

Tunnel Oxide Passivated Contact (TOPCon) Processing

One technology which shows promise of meeting the growing demands of solar panel quantity, performance and cost-effectiveness is TOPCon, or tunnel oxide passivated contact, technol ...
Page 1 of 10