Language Selector
Product Comparison

Choose products to compare anywhere you see 'Add to Compare' or 'Compare' options displayed.

Page view updated with the selected options.

Application Notes

Showing 1 - 10 of 10 Application Notes
undefined

Application Notes

Photo-Biological Testing with UV Solar Simulators

Photo-biology is the study of the effect of UVA and/or UVB, visible, and IR radiation upon living systems. The first law of photochemistry (Grotthaus-Draper Law) states that light must ...
undefined

Application Notes

Solar Simulator Dermatological Applications

Oriel® Sol-UV Solar Simulators can be used in a wide variety of dermatological applications in both new research and in commercial sun protection product verification. In commercial ...
undefined

Application Notes

Light Sources in Mars Simulation Chamber

Scientists at the Kennedy Space Center, FL used Oriel® Light Sources in their Mars Simulation Chamber (MSC). The MSC was designed to accurately maintain the pressure (7 mb). temperature ...
undefined

Application Notes

Two-Dimensional (X-Y) Stiles-Crawford Effect

Dr. Philip Kruger at the State University of New York, College of Optometry, used 100 W Quartz Tungsten Halogen Oriel® Light Sources and Optical Accessories to build a system to measure ...
undefined

Application Notes

Comparisons of IV Curves between Xenon Lamp-Based and LED-Based Solar Simulators

This note compares the IV sweep results of a Xenon lamp based solar simulator to the LED based VeraSol solar simulator. In the first section, the spectral outputs of the two simulators ...
undefined

Application Notes

Photo Biological Testing with With UV Solar Simulators

Photo-biology is the study of the effect of UVA and/or UVB, visible, and IR radiation upon living systems. The first law of photochemistry (Grotthaus-Draper Law) states that light must ...
undefined

Application Notes

Photoresponse Mapping of Photovoltaic Cells

The performance of a photovoltaic (PV) cell can be quantified by measuring its spectral response and I-V curve. From these measurements the parameters like external quantum efficiency ...
undefined

Application Notes

Reliable Solar Cell Measurements

There are five electrical performance parameters to be discussed that are used to characterize any solar cell and to compare it to other solar cells of the same or different material. ...
undefined

Application Notes

Spectroradiometric Measurements

Spectroradiometric Systems, or Spectroradiometers, measure spectral irradiance as a function of wavelength. They are typically used to measure the spectral output of an unknown or to ...
undefined

Application Notes

The Spectral Mismatch Factor

A reference solar cell is calibrated when its short-circuit current is known with respect to an internationally accepted set of test conditions called the Standard Test Conditions (1 ...