Spectra-Physics® New Industrial DPSS Lasers Span UV to IR, High Power to Compact

New high speed Pulseo 355-Turbo UV and compact infrared Explorer 1064-3 Q-switched lasers expand portfolio

Santa Clara, CA – January 24, 2012 – Spectra-Physics®, a Newport Corporation brand, introduces two new industrial Q-switched lasers for 24/7 microelectronics manufacturing applications. The Pulseo® 355-Turbo™ features advanced ultraviolet (UV) performance at very high repetition rates (up to 500 kHz), making it ideal for high-speed processing of semiconductors, touch screens, high density interconnects, and other microelectronics. The Explorer® 1064-3 delivers high infrared (IR) peak power, excellent beam quality and brightness in a robust, compact package for memory repair and micromachining applications.

“These two new lasers demonstrate the breadth and strength of the Spectra-Physics industrial DPSS laser portfolio,”

stated Herman Chui, senior director of product marketing for Spectra-Physics.

“The Pulseo 355-Turbo has higher UV power and half the noise of competing lasers, while the Explorer 1064-3 is a versatile IR laser with state-of-the-art performance in a rugged, tiny package.”

The Pulseo 355-Turbo features >8W 355nm output power with <8 percent pulse-to-pulse stability at 300 kHz repetition rate. Based on the reliable and stable Explorer platform, the Explorer 1064-3 offers short <12ns pulse widths and near diffraction-limited beam quality in a robust package that can be used on moving gantries. Both lasers are designed and manufactured to meet the highest industrial laser quality, performance, and reliability standards for demanding 24/7 applications.

Spectra-Physics’ new Pulseo 355-Turbo and Explorer 1064-3 lasers will be featured at SPIE Photonics West, The Moscone Center, San Francisco, CA, January 24-26, 2012. Please visit Newport's booth #1301 for a demonstration. For more information, please visit: www.newport.com/qsl

Company Contacts

Kim Abair
Director, Global Marketing
Tel: 800-222-6440 / 949-863-3144
Email: kim.abair at newport dot com

Herman Chui
Sr. Director of Product Marketing
Tel: 408-980-6996
Email: herman.chui at newport dot com

About Newport Corporation

Newport Corporation is a leading global supplier of advanced-technology products and systems to customers in the scientific research, microelectronics manufacturing, aerospace and defense/security, life and health sciences and precision industrial manufacturing markets. Newport's innovative solutions leverage its expertise in high-power semiconductor, solid-state and ultrafast lasers, photonics instrumentation, sub-micron positioning systems, vibration isolation, optical subsystems and precision automation to enhance the capabilities and productivity of its customers' manufacturing, engineering and research applications. Newport is part of the Standard & Poor's SmallCap 600 Index and the Russell Microcap Index.