Photonic Crystal Fiber (PCF) can provide characteristics that ordinary optical fiber do not exhibit, such as: single mode operation from the UV to IR with large mode-field diameters, highly nonlinear performance for super continuum generation, numerical aperture (NA) values ranging from very low to about 0.9, optimized dispersion properties, and air core guidance, among others. Applications for photonic crystal fibers include spectroscopy, metrology, biomedicine, imaging, telecommunication, industrial machining, and military, and the list keeps growing as the technology becomes a mainstream. Photonic crystal fibers are generally divided into two main categories: Index Guiding fibers that have a solid core, and Photonic Bandgap or air guiding fibers that have periodic micro-structured elements and a core of low index material (e.g. hollow core). A Classification tree is shown below in Fig. 1. Newport offers F-SM Series Large Mode Area, endlessly single-mode PCFs, F-NL Series Highly Nonlinear PCFs, and F-AIR Series Photonic Bandgap fibers, manufactured by Crystal Fibre, the biggest commercial supplier of photonic crystal fibers. Also offered is the SCG-800 and SCG-800-CARS self contained Supercontinuum Generators (see
Supercontinuum Generation Fiber Devices). Please refer to our Fiber Tutorial Section (see
Tutorial on Fiber Optics) for more detailed information on ...
Photonic Crystal Fiber (PCF) can provide characteristics that ordinary optical fiber do not exhibit, such as: single mode operation from the UV to IR with large mode-field diameters, highly nonlinear performance for super continuum generation, numerical aperture (NA) values ranging from very low to about 0.9, optimized dispersion properties, and air core guidance, among others. Applications for photonic crystal fibers include spectroscopy, metrology, biomedicine, imaging, telecommunication, industrial machining, and military, and the list keeps growing as the technology becomes a mainstream. Photonic crystal fibers are generally divided into two main categories: Index Guiding fibers that have a solid core, and Photonic Bandgap or air guiding fibers that have periodic micro-structured elements and a core of low index material (e.g. hollow core). A Classification tree is shown below in Fig. 1. Newport offers F-SM Series Large Mode Area, endlessly single-mode PCFs, F-NL Series Highly Nonlinear PCFs, and F-AIR Series Photonic Bandgap fibers, manufactured by Crystal Fibre, the biggest commercial supplier of photonic crystal fibers. Also offered is the SCG-800 and SCG-800-CARS self contained Supercontinuum Generators (see
Supercontinuum Generation Fiber Devices). Please refer to our Fiber Tutorial Section (see
Tutorial on Fiber Optics) for more detailed information on the properties of photonic crystal fiber. Newport's broad photonic crystal fiber selection provides the customers with the highest performance, most widely used fiber products. For adding fiber connectors and protective jackets, please contact Newport technical support.
The following volume discount schedule is automatically applied when ordering bare optical fiber: 6 - 20 m with 15 %, 21- 100 m with 22 %, > 100 m with 25 %