|  
Sign In  Or  Create New Account
  Optics
    Accessories
    Beamsplitters
    Cylindrical and Specialty Lenses
    Diffraction Gratings
    Discount Optics
    High-Energy Optics
    Mirrors
    Optical Filters
    Optical Systems
    Optics Sets
    Polarization Optics
    Prisms
    Replicated Mirrors
   
 
   
 
   
 
   
 
   
 
   
 
   
 
    Retroreflectors
    Spherical Lenses
    Technical Reference and Fundamental Applications
    Ultrafast Laser Optics
    Windows
 Show All Product Lines
Home > Products > Optics > Replicated Mirrors > Custom Ellipsoidal Replicated Mirror

Custom Ellipsoidal Replicated Mirror
Custom replicated ellipsoid mirrors provide solutions to many challenges encountered by instrument designers. These mirrors can be fabricated in an infinite number of mounting configurations which can both simplify the alignment process, and position the mirror in the most economical location in the instrument.

The specifications provided here represent the most common values for each parameter. If no alternate value is supplied, we will manufacture to these specifications.

Optic/Mount - Design Considerations:

Optical Surface

Ellipsoids can be specified in many ways including the eccentricity (e = cos a/cos b< l ), the conic constant K (K = -e2) and the vertex radius, or both the major and minor radii (x2/a2 + y2/b2 =1, where a and b are the radii). For either method, the other characteristics can be calculated such as the spacing between f1 and f2 (d = 2 (a2 -b2)1/2), or the distance from the vertex to f1 (v = a-(a2 -b2)1/2). Hyperboloids are specified similarly.The tolerances of the shape of the ellipsoid or hyperboloid are very important. The most direct approach is to tolerance the distance between the vertex and f1 , and the spacing between f1 and f2.

For an off-axis section of an ellipsoid, the center of the section must be specified as well. This can be done by specifying the angle between the axis of the ellipsoid and a ray from f1 to the ellipsoid section center. It also can be done by specifying the x-y coordinates of the center of the section relative to the ellipsoid. For either method, a tolerance must be given. By doing so, the equivalent of power will also be specified. Variation from a true ellipsoid may be given by specifying irregularity or by specifying the amount of energy in a blur circle diameter at the focal point.

Alignment

Specifying the alignment of the mounting surface to the optical surface can be somewhat simple or very complex. The first decision to be made is whether the part will be pre-aligned or aligned in assembly. If aligned in assembly, the required number of degrees of freedom must be specified. Linear displacements and rotational interactions must be considered when aligning aspherics. Aspherics such as ellipsoids, are further complicated by having an object point and an image point. To reflect the light from the object onto the image plane using a fixed mount for these aspherics is impractical unless the resolution requirements are somewhat loose. Still, it is practical to provide alignment of the mounting surface for some degrees of freedom and provide adjustment for others. A linear adjustment on an ellipsoid may cause some acceptable level of deterioration in resolution while still locating the image plane in the correct position.



Surface/Coating Quality 80/50; F/F per MIL-F-48616 (typical)
Surface Roughness 25Å rms (typical)
Power λ/4 pv @ 633nm (typical)
Irregularity λ/4 pv @ 633nm (typical)
Coating Aluminum overcoated with SiO (typical)
Reflectance ≥85% (avg) 400 - 800nm (typical)
Radius tolerance ±1.0% (typical)


 
Founded in 1969, Newport is a pioneering single-source solutions provider of laser and photonics components to the leaders in scientific research, life and health sciences, photovoltaics, microelectronics, industrial manufacturing, and homeland security markets.
Home | Products | Support | Markets | About Us | Investors | My Account | Contact Us | Contact Webmaster
Terms of Use | Privacy Policy   Copyright © 1996-2009 Newport Corporation. All rights reserved .