var decimalPointDelimiter = "."
var defaultEmptyOK = false
// Check whether string s is empty.

function isEmpty(s)
{   
	return ((s == null) || (s.length == 0))
}

// Returns true if character c is a digit 
// (0 .. 9).
function isDigit (c)
{   return ((c >= "0") && (c <= "9"))
}

// isFloat (STRING s [, BOOLEAN emptyOK])
// 
// True if string s is an unsigned floating point (real) number. 
//
// Also returns true for unsigned integers. If you wish
// to distinguish between integers and floating point numbers,
// first call isInteger, then call isFloat.
//
// Does not accept exponential notation.
//
// For explanation of optional argument emptyOK,
// see comments of function isInteger.

function isFloat (s)
{   var i;
    var seenDecimalPoint = false;

    if (isEmpty(s)) 
       if (isFloat.arguments.length == 1) return defaultEmptyOK;
       else return (isFloat.arguments[1] == true);

    if (s == decimalPointDelimiter) return false;

    // Search through string's characters one by one
    // until we find a non-numeric character.
    // When we do, return false; if we don't, return true.

    for (i = 0; i < s.length; i++)
    {   
        // Check that current character is number.
        var c = s.charAt(i);

        if ((c == decimalPointDelimiter) && !seenDecimalPoint) seenDecimalPoint = true;
        else if (!isDigit(c)) return false;
    }

    // All characters are numbers.
    return true;
}


// isSignedFloat (STRING s [, BOOLEAN emptyOK])
// 
// True if string s is a signed or unsigned floating point 
// (real) number. First character is allowed to be + or -.
//
// Also returns true for unsigned integers. If you wish
// to distinguish between integers and floating point numbers,
// first call isSignedInteger, then call isSignedFloat.
//
// Does not accept exponential notation.
//
// For explanation of optional argument emptyOK,
// see comments of function isInteger.

function isSignedFloat (s)

{   if (isEmpty(s)) 
       if (isSignedFloat.arguments.length == 1) return defaultEmptyOK;
       else return (isSignedFloat.arguments[1] == true);

    else {
        var startPos = 0;
        var secondArg = defaultEmptyOK;
        if (isSignedFloat.arguments.length > 1)
            secondArg = isSignedFloat.arguments[1];

        // skip leading + or -
        if ( (s.charAt(0) == "-") || (s.charAt(0) == "+") )
           startPos = 1;    
        return (isFloat(s.substring(startPos, s.length), secondArg))
    }
}

function CheckValues(objSource, objArgs)
{
	if(isSignedFloat(objArgs.Value) == false)
		objArgs.IsValid = false;
	else
		objArgs.IsValid = true;
}