Newport offers a wide variety of spherical and aspherical lenses made from BK 7, UV grade fused silica, Infrared grade Calcium Fluoride (CaF2), Magnesium Fluoride (MgF2), AMTR and Zinc Selenide materials. For applications in the visible and infrared up to about 2.1 µm, BK 7 offers excellent performance at a good value. In the ultraviolet down to 195 nm, UV fused silica is a good choice. UV fused silica also has excellent transmission in the visible and infrared up to about 2.1 µm, better homogeneity, and a lower coefficient of thermal expansion than BK 7. CaF2 and MgF2 are excellent choices for deep UV or infrared applicationsfor custom applications, Newport can provide quotes on a build-to-print basis.
For common optical materials, this technical note offers specifications for important basic parameters such as index of refraction, transmission across various wavelength ranges, reflectance, Abbe Number, coefficient of thermal expansion, conductivity, heat capacity, density, Knoop hardness, and Young's modulus.
Also see Optical Material Properties, for additional information.
BK 7
BK 7 is one of the most common borosilicate crown glasses used for visible and near infrared optics. Its high homogeneity, low bubble and inclusion content, and straightforward manufacturability make it a good choice for transmissive optics. BK7 is also relatively hard and shows good scratch resistance. The transmission range for BK 7 is 3802100 nm. It is not recommended for temperature sensitive applications, such as precision mirrors.

UV Grade Fused Silica
UV Grade Fused Silica is synthetic amorphous silicon dioxide of extremely high purity. This non-crystalline, colorless silica glass combines a very low thermal expansion coefficient with good optical qualities, and excellent transmittance in the ultraviolet region down to 195 nm. Transmission and homogeneity exceed those of crystalline quartz without the problems of orientation and temperature instability inherent in the crystalline form. Fused silica is ideally used with high-energy lasers due to its high energy damage threshold. UV fused silica also has excellent transmission in the visible and infrared region up to approximately 2.1 µm, and a low content of inclusions with high refractive index homogeneity. Fused silica is used for both transmissive and reflective optics, especially where high laser damage threshold is required.

CaF2
Calcium Fluoride is a cubic single crystal material grown using the vacuum Stockbarger Technique with good vacuum UV to infrared transmission. CaF2 has a wide spectral range and is an excellent choice for deep UV to infrared applications because of its non-birefringent properties. CaF2 has a transmission above 90% between 0.25 and 7µm, and is commonly used for excimer laser optics due to its low absorption and high damage threshold. Material for IR use is grown using naturally mined fluorite, at much lower cost. CaF2 has very poor thermal properties with its high coefficient of thermal expansion, and should be avoided in high operating temperature environment. Calcium fluoride can be used without an Anti-Reflection coating due to its low index of refraction.

MgF2
Magnesium Fluoride is a positive birefringent crystal grown using the vacuum Stockbarger Technique with good vacuum UV to infrared transmission. It is typically oriented with the c axis parallel to the optical axis to reduce birefringent effects. MgF2 is another excellent choice for deep UV to infrared regions, with good transmission range from 0.15 µm to 6.5 µm, and its proven use in fluorine environments make it ideal for lenses, windows, and polarizers for Excimer lasers. MgF2 is resistant to the thermal and mechanical shock, and has higher energy damage threshold. MgF2 is one of the lowest index infrared materials, which usually doesnt require anti-reflection coating. MgF2 is extremely durable compared to other materials which are transparent from the UV to the IR spectrum. MgF2 is an ideal choice for many biological and military imaging applications that require wide broadband laser pulses.

Crystal Quartz
Crystal Quartz is a positive uniaxial birefringent single crystal grown using a hydrothermal process. It has good transmission from the vacuum UV to the near infrared. Due to its birefringent nature, crystal quartz is commonly used for wave plates.

Pyrex®
Pyrex® is a borosilicate glass with a low coefficient of thermal expansion. It is mainly used for non-transmissive optics, such as mirrors, due to its low homogeneity and high bubble content.
Zerodur®
Zerodur® is a glass ceramic material that has a coefficient of thermal expansion approaching zero, as well as excellent homogeneity of this coefficient throughout the entire piece. This makes Zerodur ideal for mirror substrates where extreme thermal stability is required. Zerodur should not be used for transmissive optics due to inclusions in the material.
ZnSe
Zinc selienide is a chemically vapor deposited material commonly used in thermal imaging and medical systems. ZnSe is an excellent choice for IR lens with its broad wavelength range (600nm- 16 µm). ZnSe has a high index of refraction which normally requires an anti-reflection coating to achieve high transmission. ZnSe is relatively soft with low scratch resistance thus not recommended for use in harsh environment. Extra caution is required during cleaning, handling, and mounting. ZnSe is the best choice for optics used in high power CO2 laser systems due to its low absorption coefficient and high resistance to thermal shock.
Properties of Optical Materials
|
Abbe Number vd |
Coefficient of Thermal Expansion (10-6/°C) |
Conductivity (W/m°C) |
Heat Capacity (J/gm°C) |
Density at 25°C (gm/cm3) |
Knoop Hardness (kg/mm2) |
Youngs Modulus (GPa) |
| BK 7 |
64.17 |
7.1 |
1.114 |
0.858 |
2.51 |
610 |
81.5 |
| SF 2 |
33.85 |
8.4 |
0.735 |
0.498 |
3.86 |
410 |
55 |
| UV Fused Silica |
67.8 |
0.52 |
1.38 |
0.75 |
2.202 |
600 |
73 |
| CaF2 |
94.96 |
18.85 |
9.71 |
0.85 |
3.18 |
158 |
75.8 |
| MgF2 |
106.18 |
13.7 || to c axis 8.48 ⊥ to c axis |
21 || to c axis 30 to ⊥ c axis |
1.024 |
3.177 |
415 |
138.5 |
| Crystal Quartz |
69.87 |
7.1 to || c axis 13.2 ⊥ to c axis |
10.4 || to c axis 6.2 ⊥ to c axis |
0.74 |
2.649 |
740 |
97 || to c axis 76.5 ⊥ to c axis |
| Pyrex® |
66 |
3.25 |
1.13 |
0.75 |
2.23 |
418 |
65.5 |
| Zerodur® |
56.09 |
0 ± 0.1 |
1.46 |
0.80 |
2.53 |
620 |
90.3 |
| ZnSe |
84.45 |
7.6 |
18.0 |
0.399 |
5.27 |
105 |
70 |
Common Optical Material Properties
| Material |
Transmission Range |
Cost |
Features |
| BK 7 |
3802100 nm |
Low |
High transmission for visible to near infrared applications, the most common optical glass |
| UV Fused Silica (UVFS) |
1952100 nm |
Moderate |
Excellent homogeneity and low thermal expansion, high laser damage resistance |
| CaF2 |
1708000 nm |
High |
High transmission for deep UV to infrared applications |
| MgF2 |
1506500 nm |
High |
Birefringent material, excellent for use in the deep UV to infrared |
| ZnSe |
60016000 nm |
High |
Excellent choice for IR lens due to its broad wavelength range. Perfect candidate to use with high power infrared laser due to its low absorption coefficient. |
Index of Refraction
Wavelength (nm) |
Source |
BK 7 |
SF 2 |
UV Fused Silica |
CaF2 |
MgF2 no |
MgF2 ne |
Crystal Quartz no |
Crystal Quartz ne |
| 193 |
ArF excimer laser |
1.65528 |
1.52127 |
1.56077 |
1.50153 |
1.42767 |
1.44127 |
1.66091 |
1.67455 |
| 244 |
Ar-Ion laser |
1.58265 |
1.98102 |
1.51086 |
1.46957 |
1.40447 |
1.41735 |
1.60439 |
1.61562 |
| 248 |
KrF excimer |
1.57957 |
1.93639 |
1.50855 |
1.46803 |
1.40334 |
1.41618 |
1.60175 |
1.61289 |
| 257 |
Ar-Ion laser |
1.57336 |
1.86967 |
1.50383 |
1.46488 |
1.40102 |
1.41377 |
1.59637 |
1.60731 |
| 266 |
Nd:YAG laser |
1.56796 |
1.82737 |
1.49968 |
1.46209 |
1.39896 |
1.41164 |
1.59164 |
1.60242 |
| 308 |
XeCl excimer laser |
1.55006 |
1.73604 |
1.48564 |
1.45255 |
1.39188 |
1.40429 |
1.57556 |
1.58577 |
| 325 |
HeCd laser |
1.54505 |
1.71771 |
1.48164 |
1.44981 |
1.38983 |
1.40216 |
1.57097 |
1.58102 |
| 337.1 |
N2 laser |
1.54202 |
1.70749 |
1.47919 |
1.44813 |
1.38858 |
1.40085 |
1.56817 |
1.57812 |
| 351 |
XeF excimer laser |
1.53896 |
1.69778 |
1.47672 |
1.44642 |
1.38730 |
1.39952 |
1.56533 |
1.57518 |
| 351.1 |
Ar-Ion laser |
1.53894 |
1.69771 |
1.47671 |
1.44641 |
1.38729 |
1.39951 |
1.56531 |
1.57516 |
| 354.7 |
Nd:YAG laser |
1.53821 |
1.69548 |
1.47612 |
1.44601 |
1.38699 |
1.39920 |
1.56463 |
1.57446 |
| 363.8 |
Ar-Ion laser |
1.53649 |
1.69029 |
1.47472 |
1.44504 |
1.38626 |
1.39844 |
1.56302 |
1.57279 |
| 404.7 |
Mercury arc, h line |
1.53023 |
1.67263 |
1.46961 |
1.44151 |
1.38360 |
1.39567 |
1.55714 |
1.56670 |
| 416 |
Kr-Ion laser |
1.52885 |
1.66893 |
1.46847 |
1.44072 |
1.38301 |
1.39505 |
1.55583 |
1.56535 |
| 435.8 |
Mercury arc,g line |
1.52669 |
1.66331 |
1.46670 |
1.43949 |
1.38207 |
1.39408 |
1.55379 |
1.56323 |
| 441.6 |
HeCd laser |
1.52611 |
1.66184 |
1.46622 |
1.43916 |
1.38183 |
1.39382 |
1.55324 |
1.56266 |
| 457.9 |
Ar-Ion laser |
1.52461 |
1.65807 |
1.46498 |
1.43830 |
1.38118 |
1.39314 |
1.55181 |
1.56119 |
| 465.8 |
Ar-Ion laser |
1.52395 |
1.65641 |
1.46443 |
1.43792 |
1.38088 |
1.39284 |
1.55118 |
1.56053 |
| 472.7 |
Ar-Ion laser |
1.52339 |
1.65505 |
1.46397 |
1.43760 |
1.38064 |
1.39258 |
1.55065 |
1.55998 |
| 476.5 |
Ar-Ion laser |
1.52309 |
1.65432 |
1.46372 |
1.43744 |
1.38051 |
1.39245 |
1.55036 |
1.55969 |
| 480 |
Cadmium arc, F line |
1.52283 |
1.65367 |
1.46350 |
1.43728 |
1.38040 |
1.39233 |
1.55011 |
1.55943 |
| 486.1 |
Hydrogen arc, F line |
1.52238 |
1.65258 |
1.46313 |
1.43703 |
1.38020 |
1.39212 |
1.54968 |
1.55898 |
| 488 |
Ar-Ion laser |
1.52224 |
1.65225 |
1.46301 |
1.43695 |
1.38014 |
1.39206 |
1.54955 |
1.55885 |
| 496.5 |
Ar-Ion laser |
1.52165 |
1.65083 |
1.46252 |
1.43661 |
1.37988 |
1.39179 |
1.54898 |
1.55826 |
| 501.7 |
Ar-Ion laser |
1.52130 |
1.65000 |
1.46223 |
1.43641 |
1.37973 |
1.39163 |
1.54865 |
1.55792 |
| 510.6 |
Cu vapor laser |
1.52073 |
1.64865 |
1.46176 |
1.43609 |
1.37948 |
1.39137 |
1.54810 |
1.55735 |
| 514.5 |
Ar-Ion laser |
1.52049 |
1.64808 |
1.46156 |
1.43595 |
1.37937 |
1.39126 |
1.54787 |
1.55711 |
| 532 |
Nd:YAG laser |
1.51947 |
1.64570 |
1.46071 |
1.43537 |
1.37892 |
1.39079 |
1.54689 |
1.55610 |
| 543.5 |
HeNe laser |
1.51886 |
1.64427 |
1.46019 |
1.43502 |
1.37865 |
1.39051 |
1.54630 |
1.55549 |
| 546.1 |
Mercury arc, e line |
1.51872 |
1.64397 |
1.46008 |
1.43494 |
1.37859 |
1.39044 |
1.54617 |
1.55535 |
| 578.2 |
Cu vaport laser |
1.51720 |
1.64053 |
1.45880 |
1.43408 |
1.37792 |
1.38974 |
1.54470 |
1.55383 |
| 587.6 |
Helium arc, d line |
1.51680 |
1.63963 |
1.45846 |
1.43385 |
1.37774 |
1.38956 |
1.54431 |
1.55343 |
| 589.3 |
Sodium arc, D line |
1.51673 |
1.63947 |
1.45840 |
1.43381 |
1.37771 |
1.38952 |
1.54424 |
1.55336 |
| 594.1 |
HeNe laser |
1.51653 |
1.63904 |
1.45824 |
1.43370 |
1.37762 |
1.38943 |
1.54405 |
1.55316 |
| 611.9 |
HeNe laser |
1.51584 |
1.63752 |
1.45765 |
1.43331 |
1.37732 |
1.38911 |
1.54337 |
1.55247 |
| 628 |
Ruby laser |
1.51526 |
1.63626 |
1.45716 |
1.43298 |
1.37706 |
1.38884 |
1.54281 |
1.55188 |
| 632.8 |
HeNe laser |
1.51509 |
1.63590 |
1.45702 |
1.43289 |
1.37698 |
1.38876 |
1.54264 |
1.55171 |
| 635 |
Laser diode |
1.51501 |
1.63574 |
1.45695 |
1.43284 |
1.37695 |
1.38873 |
1.54257 |
1.55164 |
| 643.8 |
Cadmium arc, C' line |
1.51472 |
1.63512 |
1.45671 |
1.43268 |
1.37682 |
1.38859 |
1.54228 |
1.55134 |
| 647.1 |
Kr-Ion laser |
1.51461 |
1.63489 |
1.45661 |
1.43262 |
1.37677 |
1.38854 |
1.54218 |
1.55123 |
| 650 |
Laser diode |
1.51452 |
1.63469 |
1.45653 |
1.43257 |
1.37673 |
1.38850 |
1.54209 |
1.55114 |
| 656.3 |
Hydrogen arc, C line |
1.51432 |
1.63427 |
1.45637 |
1.43246 |
1.37664 |
1.38840 |
1.54189 |
1.55093 |
| 670 |
Laser diode |
1.51391 |
1.63340 |
1.45601 |
1.43223 |
1.37646 |
1.38821 |
1.54148 |
1.55051 |
| 676.4 |
Kr-Ion laser |
1.51372 |
1.63301 |
1.45585 |
1.43212 |
1.37637 |
1.38812 |
1.54130 |
1.55032 |
| 694.3 |
Ruby laser |
1.51322 |
1.63198 |
1.45542 |
1.43185 |
1.37615 |
1.38789 |
1.54080 |
1.54981 |
| 750 |
Laser diode |
1.51184 |
1.62922 |
1.45424 |
1.43109 |
1.37553 |
1.38724 |
1.53943 |
1.54839 |
| 780 |
Laser diode |
1.51118 |
1.62796 |
1.45367 |
1.43074 |
1.37524 |
1.38693 |
1.53878 |
1.54771 |
| 830 |
Laser diode |
1.51020 |
1.62613 |
1.45282 |
1.43023 |
1.37480 |
1.38647 |
1.53779 |
1.54668 |
| 850 |
Laser diode |
1.50984 |
1.62548 |
1.45250 |
1.43004 |
1.37464 |
1.38630 |
1.53742 |
1.54630 |
| 852.1 |
Cesium arc, s line |
1.50980 |
1.62541 |
1.45247 |
1.43002 |
1.37462 |
1.38628 |
1.53739 |
1.54626 |
| 905 |
Laser diode |
1.50892 |
1.62387 |
1.45168 |
1.42957 |
1.37422 |
1.38586 |
1.53648 |
1.54532 |
| 980 |
Laser diode |
1.50779 |
1.62202 |
1.45067 |
1.42902 |
1.37371 |
1.38533 |
1.53531 |
1.54409 |
| 1014 |
Mercury arc, t line |
1.50731 |
1.62128 |
1.45024 |
1.42879 |
1.37350 |
1.38510 |
1.53481 |
1.54357 |
| 1053 |
Nd:YLF laser |
1.50678 |
1.62049 |
1.44976 |
1.42854 |
1.37326 |
1.38485 |
1.53425 |
1.54299 |
| 1060 |
Nd:Glass laser |
1.50669 |
1.62035 |
1.44968 |
1.42850 |
1.37322 |
1.38480 |
1.53415 |
1.54288 |
| 1064 |
Nd:YAG laser |
1.50663 |
1.62028 |
1.44963 |
1.42848 |
1.37319 |
1.38478 |
1.53410 |
1.54282 |
| 1300 |
Laser diode |
1.50370 |
1.61644 |
1.44692 |
1.42721 |
1.37188 |
1.38338 |
1.53094 |
1.53950 |
| 1320 |
Nd:YAG laser |
1.50346 |
1.61616 |
1.44669 |
1.42711 |
1.37177 |
1.38327 |
1.53068 |
1.53922 |
| 1550 |
Laser diode |
1.50065 |
1.61312 |
1.44402 |
1.42602 |
1.37052 |
1.38194 |
1.52761 |
1.53596 |
| 1970.1 |
Mercury arc |
1.49495 |
1.60780 |
1.43852 |
1.42401 |
1.36803 |
1.37928 |
1.52138 |
1.52932 |
| 2100 |
Ho:YAG laser |
1.49296 |
1.60608 |
1.43659 |
1.42334 |
1.36718 |
1.37837 |
1.51924 |
1.52703 |
| 2325.4 |
Mercury arc |
1.48921 |
1.60291 |
1.43293 |
1.42212 |
1.36559 |
1.37667 |
1.51524 |
1.52277 |
| 2940 |
Er:YAG laser |
1.47670 |
1.59273 |
1.42065 |
1.41827 |
1.36051 |
1.37123 |
1.50246 |
1.50908 |
Transmittance of Optical Materials
These graphs compare the transmission of standard optical materials. The transmission values listed here are equivalent to "external transmittance" and takes into consideration the reflectances you get from uncoated optical elements.
Transmission of 10 mm thick fused silica, BK7, and crown glass windows.
Transmittance of IR optical materials.
Transmittance of UV-IR materials.
Transmittance of VIS-NIR materials.Reflectance of Optical Materials
All metal reflectors deteriorate slowly in polluted atmosphere. Cumulative exposure to intense ultraviolet radiation also affects performance; overheating of the reflective surface will destroy the reflector.
Typical near normal incidence reflectance of freshly deposited Al, AlMgF2, AlSiO, and Au.
Typical near normal incidence reflectance of Rhodium, enhanced Rhodium, and Silver with Dielectric orvercoat.The enhanced rhodium coating has been optimized for high performance in the ultraviolet, a wide range of angles of incidence and longevity. It is the most efficient and durable coating available for ellipsoidal reflectors. The AlMgF2 coating has been optimized for performance in the near UV.