Irvine, CA May 22, 2012 Newport Corporation, a worldwide leader in laser and photonic solutions that Make, Manage and Measure Light®, introduces the SR-Series Magnetic Optical Support Rods for mounting components to an optical table. The new, 1.5-inch diameter stainless steel rods are exceptionally stable and rigid, making them ideal for large optical mounts. For added flexibility, each pedestal rod has two sizes of threaded mounting holes (8-32/M4 and ¼-20/M6) which double their utility.
The SR-Z rods feature graduated height marks and an integrated, high-strength magnet in the pedestal base. The all-stainless steel clamping fork makes it easy and convenient to clamp the rods to any optical table. Accessories include the SR-E threaded extension rods, the SR-S spacers, the SR-Q mounting cube and thread adaptor, the SR-SC sliding clamp, and the SR-ADP mounting adaptor. Using the SR-ADP mounting adaptor, components such as mirror mounts can be rod-mounted at varying and non-standard heights. If pedestal mounting is needed without the magnetic base, Newports SR-B pedestal base is available which can be combined with the SR-E extension posts, SR-S spacers and the SR-ADP for multiple height configurations.
Newports optical support rods are available in both English and metric thread options. For more information about the SR-Series Magnetic Base Optical Support Rods and compatible accessories, please visit: www.newport.com/SR-Series
Company Contacts
Kim Abair
Director, Global Marketing
Tel: 800-222-6440 / 949-863-3144
Email: kim.abair at newport dot com
Rick Sebastian
Sr. Manager, Product Marketing
Tel: 949-437-9935
E-mail: rick.sebastian@newport.com
About Newport Corporation
Newport Corporation is a leading global supplier of advanced-technology products and systems to customers in the scientific research, microelectronics manufacturing, aerospace and defense/security, life and health sciences and precision industrial manufacturing markets. Newport's innovative solutions leverage its expertise in high-power semiconductor, solid-state and ultrafast lasers, photonics instrumentation, sub-micron positioning systems, vibration isolation, optical subsystems and precision automation to enhance the capabilities and productivity of its customers' manufacturing, engineering and research applications. Newport is part of the Standard & Poor's SmallCap 600 Index and the Russell Microcap Index.