Irvine, CA May 18, 2011 Newport Corporation, a worldwide leader in lasers and photonics solutions that Make, Manage and Measure Light®, introduces the first set in a series of ultrafast variable attenuators. Compact, robust, and easy-to-use, the ultrafast attenuators are available in manual (UVA-800-M) and motorized (UVA-800-CONEX) versions. The new attenuators are designed to address the challenge of safely attenuating the output of ultrafast amplifiers.
The new models of ultrafast variable attenuators are composed of specially designed thin film polarizers, zero-order achromatic waveplates, and high-precision opto-mechanics, enclosed in shuttered housings. Specially designed high-damage threshold, thin-film polarizers are pre-aligned in the sealed housing to minimize exposure to dust and other contaminants. The thin-film polarizers are utilized in conjunction with a half-waveplate providing continuously adjustable intensity ratio splitting of the dual S- and P-polarized outputs.
The P-polarized output passes through the first polarizer with negligible beam deviation and minimal dispersion. The S-polarized output is reflected off two polarizers in a parallel offset (1-in.) from the fundamental, with negligible dispersion. Both outputs have high polarization contrast ratios (greater than 1:450) and require no adjustment over the entire working range. For added functionality, the sealed housing includes a manual shutter for the S-polarized port and a removable beam dump on the P-polarized port.
The motorized version rotational stage has an integrated CONEX controller/driver, which is powered and communicates with a computer via USB port. A free NSTRUCT applet to control the stage is available for download from Newports website.
For additional information, please contact Newports Technology and Applications Center: www.newport.com/TAC
Company Contacts
Kim Abair
Director, Global Marketing
Tel: 800-222-6440 / 949-863-3144
Email: kim.abair at newport dot com
Ruben Zadoyan
Sr. Director, Technology & Applications Center
Tel: 949-253-1922
Email: ruben.zadoyan at newport dot com
About Newport Corporation
Newport Corporation is a leading global supplier of advanced-technology products and systems to customers in the scientific research, microelectronics manufacturing, aerospace and defense/security, life and health sciences and precision industrial manufacturing markets. Newport's innovative solutions leverage its expertise in high-power semiconductor, solid-state and ultrafast lasers, photonics instrumentation, sub-micron positioning systems, vibration isolation, optical subsystems and precision automation to enhance the capabilities and productivity of its customers' manufacturing, engineering and research applications. Newport is part of the Standard & Poor's SmallCap 600 Index and the Russell Microcap Index.