Irvine, CA October 26, 2011 Newport Corporation, a worldwide leader in lasers and photonics solutions that Make, Manage and Measure Light®, announces the 1830-R Optical Power Meter. A newly designed optical meter, the 1830-R provides a drop-in replacement for Newports legacy 1830-C Power Meter which has been widely used in fiber optic component production and testing.
The DC power measurements can be easily viewed in the 7-segment, backlit LED display. Units of W, dBm, dB, and relative measurement can be displayed in the 4 ½ digit, wide-angle view. A wide dynamic range is provided with power sensitivities down to 10 pW and full scale readings up to 2 W (detector dependent). The units built-in, audible beeping tone changes its frequency as a function of incident optical power, making it very useful when optimizing the optical beam alignment.
Other features include a USB 2.0 interface (Model 1830-R) and additional IEEE-488 (GPIB) / RS232C outputs (Model 1830-R-GPIB). For added convenience, two analog output modes, 2V into 1 M Ω and 1V into 50 Ω impedance, are also provided. The enhanced 1830-R (-GPIB) Optical Power Meters are hot-swappable among detectors, such as Newports low-power 818-series photodiodes and Newports higher-sensitivity 918D photodiode detector series. The ultraviolet (UV), silicon (Si), germanium (Ge), or indium gallium arsenide (InGaAs) detectors operate in the 200-1800 nm wavelengths.
CE and RoHS compliant, Newports 1830-R Optical Power Meter is available for shipping now. A USB memory stick with software and documents are included with each unit ordered. For more information about the new optical meter please visit: www.newport.com/1830-PR08
To review the complete Newport optical power/energy meter products, please see Newports Optical Power Meter Selection Guide at: www.newport.com/Guide
Company Contacts
Kim Abair
Director, Global Marketing
Tel: 800-222-6440 / 949-863-3144
Email: kim.abair@newport.com
Jay Jeong
Sr. Product Marketing Manager, Photonics Instruments
Tel: 949-757-2137
E-mail: jay.jeong@newport.com
About Newport Corporation
Newport Corporation is a leading global supplier of advanced-technology products and systems to customers in the scientific research, microelectronics manufacturing, aerospace and defense/security, life and health sciences and precision industrial manufacturing markets. Newport's innovative solutions leverage its expertise in high-power semiconductor, solid-state and ultrafast lasers, photonics instrumentation, sub-micron positioning systems, vibration isolation, optical subsystems and precision automation to enhance the capabilities and productivity of its customers' manufacturing, engineering and research applications. Newport is part of the Standard & Poor's SmallCap 600 Index and the Russell Microcap Index.